Skip to main content
Associate II
Nov 12, 2024 12:06 PM UTC
Solved

Not able write data to DDR after configuring PMIC

Hi,

I am working on STM32MP133FAFx . I have integrated PMIC and getting 1.35V voltage to DDR.

 I am using bare-metal environment without OS

Also configured required registers for DDR with below values for my hardware,

DDR_MSTR 0x00040401

DDR_MRCTRL0 0x00000010

DDR_MRCTRL1 0x00000000

DDR_DERATEEN 0x00000000

DDR_DERATEINT 0x00800000

DDR_PWRCTL 0x00000000

DDR_PWRTMG 0x00400010

DDR_HWLPCTL 0x00000000

DDR_RFSHCTL0 0x00210000

DDR_RFSHCTL3 0x00000000

DDR_RFSHTMG 0x0075007D

DDR_CRCPARCTL0 0x00000000

DDR_DRAMTMG0 0x12182012

DDR_DRAMTMG1 0x000A041A

DDR_DRAMTMG2 0x0608090F

DDR_DRAMTMG3 0x0050400C

DDR_DRAMTMG4 0x08040508

DDR_DRAMTMG5 0x05050403

DDR_DRAMTMG6 0x02020002

DDR_DRAMTMG7 0x00000202

DDR_DRAMTMG8 0x00001005

DDR_DRAMTMG14 0x000000A0

DDR_ZQCTL0 0xC2000040

DDR_DFITMG0 0x02060105

DDR_DFITMG1 0x00000202

DDR_DFILPCFG0 0x07000000

DDR_DFIUPD0 0xC0400003

DDR_DFIUPD1 0x00000000

DDR_DFIUPD2 0x00000000

DDR_DFIPHYMSTR 0x00000000

DDR_ADDRMAP1 0x00080808

DDR_ADDRMAP2 0x00000000

DDR_ADDRMAP3 0x00000000

DDR_ADDRMAP4 0x00001F1F

DDR_ADDRMAP5 0x07070707

DDR_ADDRMAP6 0x0F0F0707

DDR_ADDRMAP9 0x00000000

DDR_ADDRMAP10 0x00000000

DDR_ADDRMAP11 0x00000000

DDR_ODTCFG 0x06000600

DDR_ODTMAP 0x00000001

DDR_SCHED 0x00000F01

DDR_SCHED1 0x00000000

DDR_PERFHPR1 0x00000001

DDR_PERFLPR1 0x04000200

DDR_PERFWR1 0x08000400

DDR_DBG0 0x00000000

DDR_DBG1 0x00000000

DDR_DBGCMD 0x00000000

DDR_POISONCFG 0x00000000

DDR_PCCFG 0x00000010

DDR_PCFGR_0 0x00000000

DDR_PCFGW_0 0x00000000

DDR_PCFGQOS0_0 0x00100009

DDR_PCFGQOS1_0 0x00000020

DDR_PCFGWQOS0_0 0x01100B03

DDR_PCFGWQOS1_0 0x01000200

DDR_PGCR 0x01442E02

DDR_PTR0 0x00226698

DDR_PTR1 0x0413A980

DDR_PTR2 0x042D7700

DDR_ACIOCR 0x10400812

DDR_DXCCR 0x00000C40

DDR_DSGCR 0xF200011F

DDR_DCR 0x0000000B

DDR_DTPR0 0x34B288D0

DDR_DTPR1 0x097D00C0

DDR_DTPR2 0x10023200

DDR_MR0 0x00000840

DDR_MR1 0x00000000

DDR_MR2 0x00000208

DDR_MR3 0x00000000

DDR_ODTCR 0x00010000

DDR_ZQ0CR1 0x00000038

DDR_DX0GCR 0x0000CE81

DDR_DX1GCR 0x0000CE81

 

Also used below steps to configure

1. RESETS: presetn, core_ddrc_rstn, aresetn
2. Enable clock
3. Deassert reset
4. Delay
5. Initialize registers
6. Deassert reset signal core_ddrc_rstn, aresetn and presetn
7. Start PHY init by accessing relevant PUBL registers
8. Monitor PHY init status by polling PUBL register PGSR.IDONE
9. Indicate to PUBL that controller performs SDRAM initialization
10.SET DFIMISC INIT Complete flag to 1
11. Wait for DWC_ddr_umctl2 to move to normal operation mode
12. Disable Auto refresh and power down
12. Program PUBL PGCR to enable refresh during training and rank to train
14. Configure PUBL PIR register to run training step
15. Monitor PUB PGSR.IDONE to poll completion of training sequence
16. Enable auto refresh

 

But I am not able to access the DDR memory which is from 0xC0000000. When I am trying to access memory, processor is behaving abnormal

Please help me how to resolve this issue and provide me the solution.

 

This topic has been closed for replies.
sandeepBJadhavBest answer
Associate II
Nov 14, 2024 5:03 AM UTC

Hi,

I am able to resolve the issue by doing TZ_init(), before initializing PMIC. Then I am able to access DDR

 

3 replies

PatrickF
ST Employee
Nov 12, 2024 12:35 PM UTC

Hi @sandeepBJadhav ,

did you use the provided ddr_init sequence from https://wiki.st.com/stm32mpu/wiki/STM32CubeMP13_Package ?

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Associate II
Nov 12, 2024 12:47 PM UTC

Hi,

thanks for response.

Yes, I am using same sequence as per STM32MP13 package

sandeepBJadhavAuthorBest answer
Associate II
Nov 14, 2024 5:03 AM UTC

Hi,

I am able to resolve the issue by doing TZ_init(), before initializing PMIC. Then I am able to access DDR