Associate II
January 15, 2021
Question
Multiple Rpmsg Channels
- 1 reply
- 1884 views
Hi,
i just implemented the OpenAMP_tty_echo example for my device. And i just wanna know if i have the right understanding for it. Iam using two virtualUARTS, does this mean that i have two Endpoints over one RPMSG Channel. Or do i have two RPMSG Channel with one endpoint at one Channel? In my Undertsanding i have one RPMSG Channel with two Endpoints VirtUART0 and VirtUART1. Is there any use case to have multiple RPMSG Channels for communicating between the A7 and M4 (like shown in the picture)? And how i could integrate it? I should have another vdev device with again seperated Memory in the Shared Memory. Is my understanding correct in this cases?
Thanks so far