Skip to main content
Associate II
Aug 24, 2026 9:22 AM UTC
Question

MB1854B camera suddenly failed and is unusable.

The MB1854B camera on the STM32MP257FDK fails to open; clicking the camera icon on the desktop results in a white screen. Is this related to hot-plugging the camera? How can this be resolved?

 

dmesg -w log:
stm32-csi 48020000.csi: Timeout waiting for VC0 stop
stm32-csi 48020000.csi: Failed to stop stream:0

6 replies

Erwan SZYMANSKI
ST Technical Moderator
Aug 24, 2026 1:52 PM UTC

Hello ​@Cedricl ,
When you talk about “hot-plugging” the camera what do you mean ? Is the camera not working anymore since you hot-plugged it when the board was running ? Or do you mean that the camera cannot work properly when you hot-plug it at runtime, but can work if it is already plugged when starting the board ?

Thank you to precise.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CedriclAuthor
Associate II
Aug 25, 2026 1:24 AM UTC

Hello ​@Erwan SZYMANSKI ,

"Hot-swapping" here refers to unplugging and then replugging the camera while the board is powered on; after rebooting the device, the camera fails to function correctly. However, if I connect a known-working camera while the board is powered off, it operates normally after the board boots up—though if I subsequently accidentally hot-swap that camera, it also stops working properly.

I tried unplugging it overnight, but it still won't work properly.

 

Kind regards,

Cedricl.

 

Erwan SZYMANSKI
ST Technical Moderator
Aug 25, 2026 6:13 AM UTC

Hello ​@Cedricl,

The CSI connector present on DK board has not been imagined to be hot plugged, as the pins are really close to each other (you can see it). I guess you damaged your camera by touching some wrong connection when you removed / plugged it at runtime.

Sorry for that, but I think you need to replace the camera and do not continue to hot plug new ones. 

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Visitor
Aug 25, 2026 6:07 AM UTC

The VC0 stop timeout suggests the CSI stream may not be shutting down properly. If this happened after hot-plugging, I’d try a full power cycle and reconnect the camera while powered off. Checking dmesg after reconnecting may also help identify whether it’s a driver or hardware issue.

CedriclAuthor
Associate II
Aug 25, 2026 9:14 AM UTC

Hello ​@erajbrooks ,

 

When the camera is completely powered off and restarted, it doesn’t work properly, and reconnecting it while the device is off doesn’t help either.

However, the second camera would show a white screen during the first few hot swaps, and doing this sometimes brought it back to normal before it completely 'broke.' But after one of these times, it completely 'broke'.

 

Kind regards,

Cedricl.