Skip to main content
EAlex.1
Associate
Nov 13, 2020 12:54 PM UTC
Solved

local build TF-A crashes during boot, STM32MP157A-DK1 kit

Hello

i'm trying to get started with the STM32MP1 env, and I'm having some issues building the trusted firmware boot image, after following the steps from: https://wiki.st.com/stm32mpu/wiki/STM32MP15_TF-A

I'm, building it with the following commands, on the v2.2-stm32mp branch, with gcc version 9.3.0 (Ubuntu 9.3.0-17ubuntu1~20.04) , no changes on the git branch:

make distclean
 
make CROSS_COMPILE=arm-linux-gnueabihf- ARCH=aarch32 ARM_ARCH_MAJOR=7 PLAT=stm32mp1 DTB_FILE_NAME=stm32mp157a-dk1.dtb FDT_SOURCES=fdts/stm32mp157a-dk1.dts DEBUG=1 STM32MP_SDMMC=1 dtbs
 
make CROSS_COMPILE=arm-linux-gnueabihf- ARCH=aarch32 ARM_ARCH_MAJOR=7 PLAT=stm32mp1 DTB_FILE_NAME=stm32mp157a-dk1.dtb FDT_SOURCES=fdts/stm32mp157a-dk1.dts DEBUG=1 STM32MP_SDMMC=1

I can see the following messages on the serial console:

NOTICE: CPU: STM32MP157AAC Rev.B
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
NOTICE: Board: MB1272 Var1.0 Rev.C-01
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: PMIC version = 0x10
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.2-r2.0(debug):v2.2-stm32mp-r2
NOTICE: BL2: Built : 11:17:04, Nov 13 2020
INFO: Using crypto library 'stm32_crypto_lib'
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2 runs SP_MIN setup
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffeb000
INFO: Image id=4 loaded: 0x2ffeb000 - 0x2ffff000
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: STM32 Image size : 903902
INFO: Image id=5 loaded: 0xc0100000 - 0xc01dcade
WARNING: Skip signature check (header option)
NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffeb000
INFO: SPSR = 0x1d3
 
Undefined instruction at: 0x2ffeb00c
 
Undefined instruction at: 0x2ffd4370
 

The SD-CARD image is build with create_sdcard_from_flashlayout.sh, based on the following script:

#Opt	Id		Name		Type		IP		Offset		Binary
-		0x01	fsbl1-boot	Binary		none	0x0			arm-trusted-firmware/tf-a-stm32mp157a-dk1-serialboot.stm32
-		0x03	ssbl-boot	Binary		none	0x0			bootloader/u-boot.stm32
P		0x04	fsbl1		Binary		mmc0	0x00004400	arm-trusted-firmware/tf-a.stm32
P		0x05	fsbl2		Binary		mmc0	0x00044400	arm-trusted-firmware/tf-a.stm32
PD		0x06	ssbl		Binary		mmc0	0x00084400	bootloader/u-boot.stm32
P		0x07	boot		System		mmc0	0x00284400	st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P		0x08	rootfs		FileSystem	mmc0	0x05284400	st-image-weston-openstlinux-weston-stm32mp1.ext4

U_BOOT (also local build) and the other images are ok, as it will boot properly if I use tf-a-stm32mp157a-dk1-trusted.stm32 instead of the locally compiled binary

Are there any knows issues regarding TF-A build ?

I can't see anything related to the GCC version in https://wiki.st.com/stm32mpu/wiki/PC_prerequisites

(edit reason: wrong gcc version)

Thanks,

Alexandru

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Nov 16, 2020 2:52 PM UTC

Hi @EAlex.1​ ,

I'm a bit surprise by your build command and value of CROSS_COMPILE

Simple command line to properly buid a TF-A in provided SDK is :

make -f Makefile.sdk TF_A_CONFIG=trusted TFA_DEVICETREE=<board>

I guess you should rather look at page :

https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Building_and_deploying_the_TF-A_for_the_first_time

Rather than https://wiki.st.com/stm32mpu/wiki/STM32MP15_TF-A which expose a solution for expert likely more error prone.

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Nov 16, 2020 2:52 PM UTC

Hi @EAlex.1​ ,

I'm a bit surprise by your build command and value of CROSS_COMPILE

Simple command line to properly buid a TF-A in provided SDK is :

make -f Makefile.sdk TF_A_CONFIG=trusted TFA_DEVICETREE=<board>

I guess you should rather look at page :

https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Building_and_deploying_the_TF-A_for_the_first_time

Rather than https://wiki.st.com/stm32mpu/wiki/STM32MP15_TF-A which expose a solution for expert likely more error prone.

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
EAlex.1
EAlex.1Author
Associate
Nov 18, 2020 7:59 AM UTC

Thank you

i will re-read that wiki page, and in the meantime i'll use the provided binary