Skip to main content
GCici
Associate II
April 11, 2024
Question

Linux 6.1 does not get ethaddr from u-boot env

Hi,

we've upgraded our build from 5.15 to 6.1 and now the OS does not get the mac address set in uboot environment through a script. If i check the environment i can correctly see the ethaddr set via printenv. Is there something i can do in kernel config or ethernet driver?

This topic has been closed for replies.

6 replies

GCici
GCiciAuthor
Associate II
April 15, 2024

bump 

GCici
GCiciAuthor
Associate II
April 22, 2024

Bump

GCici
GCiciAuthor
Associate II
May 9, 2024

Possible that no one cares about this? I'm still on 5.15 because of this issue. Please help

Olivier GALLIEN
ST Technical Moderator
May 31, 2024

Hi @GCici ,

 

Sorry to come late in this thread. 

For sure ST care about your issue but we would need further information. 

 

Can you update status on your side ? 

 

When you said you change from 5.15 to 6.1 do you means only the kernel or the whole OSTL version including BSP ( TF-A, Uboot, OPTEE) . This is mandatory.

If you may share some logs about the issue it can surely help

 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GCici
GCiciAuthor
Associate II
May 31, 2024

Hello Olivier,

i mean the whole OSTL system, so TFA,UBOOT,OPTEE and kernel. which kind of logs do you need? 
I can say ethaddr is correctly set in u-boot environment and it shows correctly when i type printenv. When the system has started  the mac address on eth0 is different from the one set in uboot environment.

Cheers,

GC