Skip to main content
Visitor II
May 30, 2024
Question

LCD display not turning on - STM32MP135F-DK

  • May 30, 2024
  • 5 replies
  • 2158 views

 

I just received my STM32MP135F-DK in the mail today. I was able to use STM32CubeProgrammer v2.16.0 to populate the device using the Starter Package, which I downloaded from here:

https://www.st.com/en/embedded-software/stm32mp1starter.html#st-get-software

The file I downloaded was named:

en.flash-stm32mp1-openstlinux-6-1-yocto-mickledore-mp1-v23-06-21.tar.gz

And the file that I used in the STM32CubeProgrammer to download the firmware to the device was named:

FlashLayout_sdcard_stm32mp135f-dk-optee.tsv

After downloading the firmware to the device and toggling the switches to the correct mode, I powered up the device and the display never turned on. However, I was able to open a terminal on the device through the serial connection.

Everything seems to be working fine as far as the terminal is concerned. I even managed to connect the device to my home network and SSH into it.

The LCD display shows no signs of life. I've never seen the splash screen, or even a flicker out of it. There is no backlight turning on.

I tried flashing it with the Starter Package version 4.1.0 instead of 5.0.0, but I'm getting the same result.

I'd appreciate some help getting this device working. Does this sound like a hardware issue? Or perhaps the screen is defective on this device?

This topic has been closed for replies.

5 replies

Olivier GALLIEN
ST Technical Moderator
May 31, 2024

Hi @ChrisCrossCrash ,

 

This looks indeed abnormal, seems your board is defective. 

I recommand you to contact your distributor to get a new board

 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Visitor II
June 29, 2024

I got similar issue when using Starter package on STM32MP135F-DK

after booting normally and run following script to install demo package?

 

 apt-get install packagegroup-x-linux-ai
 systemctl restart weston-graphical-session.service

 

and I still get white  LCD display shows, instead of some demo in https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_Starter_package

adamli_0-1719646464896.jpeg

and here i got some red log in dmesg, but I could figure it out why

root@stm32mp1:~# dmesg
...
[ 0.002966] /cpus/cpu@0 missing clock-frequency property
...
[ 0.101268] Driver 'scmi-optee' was unable to register with bus_type 'tee' because the bus was not initialized.
...
[ 0.375816] stm32-cpufreq stm32-cpufreq: OPP-v2 not supported
...
[ 3.843204] Goodix-TS 1-005d: i2c test failed attempt 1: -6
[ 3.883183] Goodix-TS 1-005d: i2c test failed attempt 2: -6
[ 3.923043] Goodix-TS 1-005d: I2C communication failure: -6

 

 

 

 

 

Olivier GALLIEN
ST Technical Moderator
July 1, 2024

Hi @adamli ,

Can you please confirm screen was working fine prior to install x-linux-ai package ?

 

Thanks 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Olivier GALLIEN
ST Technical Moderator
July 5, 2024

Hi @ChrisCrossCrash ,

 

If the screen doesn't work properly with Starter Package out of the box it's likely and HW issue. Contact your board provider. 

 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.