Skip to main content
MLars.10
Associate II
July 27, 2020
Question

LBEE5KL1DX-883 using SDMMC3

Hello,

We are using the LBEE5KL1DX-883 WLAN+BT chip with a STM32MP157C on a custom board. The SDIO interface is routed to the SDMMC3 interface (different from the DK-2 board). However when we are probing the brcmfmac module, it cannot find the mmc0 interface it seems. It writes the following to the dmesg logs:

[ 21.319324] brcmfmac: No platform data available.

Is there anything extra which needs to be configured when using SDMMC3 as opposed to SDMMC2? Posting relevant configuration below. Thanks

mmc related dmesg logs during boot:

root@stm32mp1:~# dmesg | grep mmc
[ 0.000000] Kernel command line: root=/dev/mmcblk1p5 rootwait rw console=ttySTM0,115200
[ 1.799815] mmci-pl18x 48004000.sdmmc: allocated mmc-pwrseq
[ 1.804262] mmci-pl18x 48004000.sdmmc: Linked as a consumer to regulator.7
[ 1.810928] mmci-pl18x 48004000.sdmmc: mmc0: PL180 manf 53 rev1 at 0x48004000 irq 41,0 (pio)
[ 1.848186] mmci-pl18x 58005000.sdmmc: Linked as a consumer to regulator.7
[ 1.853931] mmci-pl18x 58005000.sdmmc: mmc1: PL180 manf 53 rev2 at 0x58005000 irq 48,0 (pio)
[ 2.005479] mmc1: host does not support reading read-only switch, assuming write-enable
[ 2.020796] mmc1: new high speed SDHC card at address aaaa
[ 2.038625] mmcblk1: mmc1:aaaa SC32G 29.7 GiB 
[ 2.162810] mmcblk1: p1 p2 p3 p4 p5 p6

/sys/kernel/debug/mmc0/ios

root@stm32mp1:/sys/kernel/debug/mmc0# cat ios
clock:		0 Hz
vdd:		0 (invalid)
bus mode:	2 (push-pull)
chip select:	0 (don't care)
power mode:	0 (off)
bus width:	0 (1 bits)
timing spec:	0 (legacy)
signal voltage:	0 (3.30 V)
driver type:	0 (driver type B)

Kernel SDMMC3 DT entry:

/* Wifi */
&sdmmc3 {
 arm,primecell-periphid = <0x10153180>;
 pinctrl-names = "default", "opendrain", "sleep";
 pinctrl-0 = <&sdmmc3_b4_pins_a>;
 pinctrl-1 = <&sdmmc3_b4_od_pins_a>;
 pinctrl-2 = <&sdmmc3_b4_sleep_pins_a>;
 non-removable;
 st,neg-edge;
 bus-width = <4>;
 vmmc-supply = <&v3v3>;
 mmc-pwrseq = <&wifi_pwrseq>;
 #address-cells = <1>;
 #size-cells = <0>;
 keep-power-in-suspend;
 status = "okay";
 
 brcmf: bcrmf@1 {
 reg = <1>;
 compatible = "brcm,bcm4329-fmac";
 }; 
};

U-Boot clock setup:

 st,pkcs = < 
 CLK_CKPER_HSE
 CLK_ETH_DISABLED
 CLK_SDMMC12_PLL4P
 CLK_STGEN_HSE
 CLK_USBPHY_HSE
 CLK_SPI2S1_DISABLED
 CLK_SPI2S23_PLL3Q
 CLK_SPI45_PCLK2
 CLK_SPI6_DISABLED
 CLK_I2C46_HSI
 CLK_SDMMC3_PLL4P
 CLK_USBO_USBPHY
 CLK_ADC_DISABLED
 CLK_CEC_DISABLED
 CLK_I2C12_DISABLED
 CLK_I2C35_DISABLED
 CLK_UART1_DISABLED
 CLK_UART24_PCLK1
 CLK_UART35_PCLK1
 CLK_UART6_DISABLED
 CLK_UART78_PCLK1
 CLK_SPDIF_DISABLED
 CLK_FDCAN_HSE
 CLK_SAI1_DISABLED
 CLK_SAI2_DISABLED
 CLK_SAI3_DISABLED
 CLK_SAI4_DISABLED
 CLK_RNG1_LSI
 CLK_LPTIM1_DISABLED
 CLK_LPTIM23_DISABLED
 CLK_LPTIM45_DISABLED
 >;

This topic has been closed for replies.

4 replies

Olivier GALLIEN
ST Technical Moderator
July 28, 2020

Hi @MLars.10​ 

You share only U-boot clock settings... should I understand you ar using basic boot ?

Else you need to check TF-A clock tree settings also.

Are you working with new V2.0 version or still V1.2 ?

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MLars.10
MLars.10Author
Associate II
July 28, 2020

Hi

Yes, we are using basic boot (no TF-A). This is using the older version of the BSP (Kernel version 4.19.4, U-Boot version 2018.11, not sure what eco-system version it's part of)

Ronte.1
Associate III
October 1, 2020

Hi

Did you find a solution for this? We are facing a similar problem. We are trying to change wlan routing to sdmmc3. We have a custom board which is based on stm32mp157c-dk2.

Mahendra Sondagar
Associate III
July 11, 2021

Hi.. @MLars.10​ did you find the solution?

We're also facing the similar issue

SDMMC3 seems unable to up!

Hi....@Community member​  any suggestions?