Skip to main content
MScho.6
Associate II
February 26, 2021
Solved

Kernel trace with custom stm32mp151c board and device tree (Workqueue: events deferred_probe_work_func)

Hi!

I have a custom board with custom device tree. As far as I can say, it works (boot over emmc) but the kernel gives a trace at the start.

[ 0.255543] debugfs: Directory 'cpu0' with parent 'opp' already present!
[ 0.261757] Unable to get STM32 DDR PMU clock
[ 0.294819] stm32-mdma 58000000.dma: STM32 MDMA driver registered
[ 0.296155] stm32-dma 48000000.dma: no dma pool: can't use MDMA: 0
[ 0.297740] stm32-dma 48000000.dma: STM32 DMA driver registered
[ 0.298366] reg11: supplied by fixed_3v3
[ 0.298741] reg18: supplied by fixed_3v3
[ 0.299068] usb33: supplied by fixed_3v3
[ 0.304778] dwc2 49000000.usb-otg: 49000000.usb-otg supply vusb_d not found, using dummy regulator
[ 0.304931] dwc2 49000000.usb-otg: 49000000.usb-otg supply vusb_a not found, using dummy regulator
[ 0.307539] debugfs: Directory 'cpu0' with parent 'opp' already present!
[ 0.307696] ------------[ cut here ]------------
[ 0.307729] WARNING: CPU: 0 PID: 16 at drivers/opp/of.c:686 _of_add_opp_table_v2+0x50c/0x5c0
[ 0.307738] Modules linked in:
[ 0.307757] CPU: 0 PID: 16 Comm: kworker/0:1 Not tainted 5.4.69-yocto-standard #1
[ 0.307766] Hardware name: STM32 (Device Tree Support)
[ 0.307787] Workqueue: events deferred_probe_work_func
[ 0.307825] [<c01104b4>] (unwind_backtrace) from [<c010c6d0>] (show_stack+0x10/0x14)
[ 0.307849] [<c010c6d0>] (show_stack) from [<c0aa6d4c>] (dump_stack+0xbc/0xd0)
[ 0.307871] [<c0aa6d4c>] (dump_stack) from [<c0122c7c>] (__warn+0xbc/0xd8)
[ 0.307890] [<c0122c7c>] (__warn) from [<c0122cfc>] (warn_slowpath_fmt+0x64/0xc4)
[ 0.307911] [<c0122cfc>] (warn_slowpath_fmt) from [<c0824c38>] (_of_add_opp_table_v2+0x50c/0x5c0)
[ 0.307932] [<c0824c38>] (_of_add_opp_table_v2) from [<c0824d20>] (dev_pm_opp_of_add_table+0x34/0x164)
[ 0.307953] [<c0824d20>] (dev_pm_opp_of_add_table) from [<c0824e88>] (dev_pm_opp_of_cpumask_add_table+0x38/0xfc)
[ 0.307973] [<c0824e88>] (dev_pm_opp_of_cpumask_add_table) from [<c082c070>] (cpufreq_init+0x104/0x304)
[ 0.307994] [<c082c070>] (cpufreq_init) from [<c0828f4c>] (cpufreq_online+0x420/0x9b4)
[ 0.308016] [<c0828f4c>] (cpufreq_online) from [<c082957c>] (cpufreq_add_dev+0x8c/0xc0)
[ 0.308036] [<c082957c>] (cpufreq_add_dev) from [<c05e86d4>] (subsys_interface_register+0xa4/0xf8)
[ 0.308057] [<c05e86d4>] (subsys_interface_register) from [<c082789c>] (cpufreq_register_driver+0x150/0x2ac)
[ 0.308078] [<c082789c>] (cpufreq_register_driver) from [<c082c314>] (dt_cpufreq_probe+0xa4/0x1b8)
[ 0.308098] [<c082c314>] (dt_cpufreq_probe) from [<c05ec514>] (platform_drv_probe+0x48/0x98)
[ 0.308117] [<c05ec514>] (platform_drv_probe) from [<c05ea360>] (really_probe+0x24c/0x488)
[ 0.308136] [<c05ea360>] (really_probe) from [<c05ea764>] (driver_probe_device+0x78/0x154)
[ 0.308154] [<c05ea764>] (driver_probe_device) from [<c05e83b0>] (bus_for_each_drv+0x84/0xd0)
[ 0.308171] [<c05e83b0>] (bus_for_each_drv) from [<c05ea074>] (__device_attach+0xf0/0x188)
[ 0.308189] [<c05ea074>] (__device_attach) from [<c05e917c>] (bus_probe_device+0x84/0x8c)
[ 0.308207] [<c05e917c>] (bus_probe_device) from [<c05e96cc>] (deferred_probe_work_func+0x84/0xc4)
[ 0.308228] [<c05e96cc>] (deferred_probe_work_func) from [<c013ce34>] (process_one_work+0x1c8/0x420)
[ 0.308248] [<c013ce34>] (process_one_work) from [<c013d2d4>] (worker_thread+0x248/0x528)
[ 0.308267] [<c013d2d4>] (worker_thread) from [<c0142670>] (kthread+0x144/0x180)
[ 0.308285] [<c0142670>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
[ 0.308295] Exception stack(0xc717bfb0 to 0xc717bff8)
[ 0.308310] bfa0: 00000000 00000000 00000000 00000000
[ 0.308326] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.308341] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.308352] ---[ end trace 872afcafb31983a3 ]---
[ 0.308802] debugfs: Directory 'cpu0' with parent 'opp' already present!
[ 0.308884] sysfs: cannot create duplicate filename '/devices/platform/cpufreq-dt'
[ 0.308903] CPU: 0 PID: 16 Comm: kworker/0:1 Tainted: G W 5.4.69-yocto-standard #1
[ 0.308911] Hardware name: STM32 (Device Tree Support)
[ 0.308929] Workqueue: events deferred_probe_work_func
[ 0.308958] [<c01104b4>] (unwind_backtrace) from [<c010c6d0>] (show_stack+0x10/0x14)
[ 0.308979] [<c010c6d0>] (show_stack) from [<c0aa6d4c>] (dump_stack+0xbc/0xd0)
[ 0.309001] [<c0aa6d4c>] (dump_stack) from [<c02f044c>] (sysfs_warn_dup+0x54/0x60)
[ 0.309021] [<c02f044c>] (sysfs_warn_dup) from [<c02f0588>] (sysfs_create_dir_ns+0xec/0xfc)
[ 0.309041] [<c02f0588>] (sysfs_create_dir_ns) from [<c0aac3ac>] (kobject_add_internal+0xb4/0x354)
[ 0.309060] [<c0aac3ac>] (kobject_add_internal) from [<c0aac6a8>] (kobject_add+0x5c/0xc8)
[ 0.309082] [<c0aac6a8>] (kobject_add) from [<c05e59fc>] (device_add+0x110/0x640)
[ 0.309104] [<c05e59fc>] (device_add) from [<c05ec2b0>] (platform_device_add+0x108/0x248)
[ 0.309125] [<c05ec2b0>] (platform_device_add) from [<c05ece4c>] (platform_device_register_full+0xd0/0x110)
[ 0.309146] [<c05ece4c>] (platform_device_register_full) from [<c082c53c>] (stm32_cpufreq_probe+0xec/0x194)
[ 0.309166] [<c082c53c>] (stm32_cpufreq_probe) from [<c05ec514>] (platform_drv_probe+0x48/0x98)
[ 0.309185] [<c05ec514>] (platform_drv_probe) from [<c05ea360>] (really_probe+0x24c/0x488)
[ 0.309204] [<c05ea360>] (really_probe) from [<c05ea764>] (driver_probe_device+0x78/0x154)
[ 0.309222] [<c05ea764>] (driver_probe_device) from [<c05e83b0>] (bus_for_each_drv+0x84/0xd0)
[ 0.309239] [<c05e83b0>] (bus_for_each_drv) from [<c05ea074>] (__device_attach+0xf0/0x188)
[ 0.309257] [<c05ea074>] (__device_attach) from [<c05e917c>] (bus_probe_device+0x84/0x8c)
[ 0.309275] [<c05e917c>] (bus_probe_device) from [<c05e96cc>] (deferred_probe_work_func+0x84/0xc4)
[ 0.309294] [<c05e96cc>] (deferred_probe_work_func) from [<c013ce34>] (process_one_work+0x1c8/0x420)
[ 0.309314] [<c013ce34>] (process_one_work) from [<c013d2d4>] (worker_thread+0x248/0x528)
[ 0.309333] [<c013d2d4>] (worker_thread) from [<c0142670>] (kthread+0x144/0x180)
[ 0.309350] [<c0142670>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
[ 0.309360] Exception stack(0xc717bfb0 to 0xc717bff8)
[ 0.309373] bfa0: 00000000 00000000 00000000 00000000
[ 0.309390] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 0.309405] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 0.309419] kobject_add_internal failed for cpufreq-dt with -EEXIST, don't try to register things with the same name in the same directory.
[ 0.310927] stm32-hash 54002000.hash: will run requests pump with realtime priority
[ 0.312665] stm32-hash 54002000.hash: Init HASH done HW ver 23 DMA mode 1
[ 0.313866] stm32-ddr-pmu: probed (ID=0x00140061 VER=0x00000010), DDR@533MHz

Thanks and Regards,

Matthias

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
February 26, 2021

To be more specific, fix is this one :

It was also nessesary to blacklist the device_id in drivers/cpufreq/cpufreq-dt-platdev.c

static const struct of_device_id blacklist[] __initconst = {

...

{ .compatible = "st,stm32mp157", },

+++ { .compatible = "st,stm32mp151", },

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

8 replies

Olivier GALLIEN
ST Technical Moderator
February 26, 2021

Hi @MScho.6​ ,

I guess you get similar issue than in this post :

https://community.st.com/s/question/0D53W000009340DSAQ/how-to-configuration-for-stm32mp151

The patch to be applied is explain in the comment marked "Best Answer" .

Proper fix will be integrated in a coming release.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
February 26, 2021

To be more specific, fix is this one :

It was also nessesary to blacklist the device_id in drivers/cpufreq/cpufreq-dt-platdev.c

static const struct of_device_id blacklist[] __initconst = {

...

{ .compatible = "st,stm32mp157", },

+++ { .compatible = "st,stm32mp151", },

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Lead
September 2, 2024

@Olivier GALLIEN 

Please add that to the next version of OpenSTLinux sources for STM32MP151. It removes at least one error.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
MScho.6
MScho.6Author
Associate II
February 26, 2021

No, I do not believe it has to do with that. The second trace is from: drivers/cpufreq/stm32-cpufreq.c:67 if that helps. We have a discrete power supply. Maybe some misconfiguration on my side there?! What are the dt nodes one should look at?

Olivier GALLIEN
ST Technical Moderator
February 26, 2021

Hi @MScho.6​ ,

Did you make a trial of the patch ?

Please provide new traces once applied

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MScho.6
MScho.6Author
Associate II
February 26, 2021

I tried and the patch did it. Thank you and have a nice weekend.