Skip to main content
Visitor II
June 28, 2023
Question

Kernel boot fails when enabling sdmmc3 in kernel and u-boot dts

  • June 28, 2023
  • 0 replies
  • 1354 views

We are trying to bringup the Wi-Fi module connected over the sdmmc3 line with the STM32MP157F based custom board. 

But it seems, when enabling the sdmmc3 lines on the kernel and u-boot dts files, the kernel boot fails on "Waiting for Keymaster device" as seen in the logs below:

SmithRay_0-1687980003350.png

This issue occurs only when the sdmmc3 is enabled in the dts, otherwise the boot is successful.

Cannot see where to look for the error!

This topic has been closed for replies.