Skip to main content
Yli.8
Associate III
November 26, 2019
Question

JTAG debug

I use jtag debugging m4 program, the following error, how should be resolved

Open On-Chip Debugger 0.10.0+dev-01124-gbfb41e6 (2018-11-16-15:23)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

debug_level: 1

cortex_a interrupt mask on

cortex_a interrupt mask on

cortex_a domain access control fixup on

cortex_a domain access control fixup on

3333

none separate

adapter speed: 5000 kHz

adapter_nsrst_assert_width: 200

adapter_nsrst_delay: 200

none srst_pulls_trst

srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst

Error: Could not find MEM-AP to control the core

ap 0 selected, csw 0x10006000

Error: Target not examined yet

undefined debug reason 7 - target needs reset

Error: Target not examined yet

Error: Could not find MEM-AP to control the core

Error: Target not examined yet

embedded:startup.tcl:24: Error: 

in procedure 'stm32mp15x.cpu2' called at file "embedded:startup.tcl", line 283

in procedure 'ocd_bouncer' 

at file "embedded:startup.tcl", line 24

Error: Target not examined yet

Error: Target not examined yet

Error: Target not examined yet

Error: Target not examined yet

This topic has been closed for replies.

4 replies

AntonioST
ST Employee
November 26, 2019

Your message does not explain the environment you are using, so I try to guess it.

I believe you are running SystemWorkbench while on the STM32MP1 is running Linux

In this configuration, you cannot load the M4 firmware through JTAG/SWD, but you need to "ask" Linux on the board to load the FW on M4,

This is done through "Debug Configuration" in SystemWorkbench. See screenshot below

0690X00000AsTJ5QAN.gif

Please also notice that SystemWorkbench is currently obsoleted.

I suggest you to switch to CubeIDE, available on ST website

Yli.8
Yli.8Author
Associate III
November 27, 2019
  • Thanks for your reply, please help to check my configuration

0690X00000AsUnpQAF.png

0690X00000AsUnfQAF.png0690X00000AsUnaQAF.png

louiey
Associate II
December 5, 2019

I have a same issue.

I'm reviewing "https://wiki.st.com/stm32mpu/wiki/STM32CubeMP1_Package" site and follow the step.

It says input eth0 ip address like as below.

0690X00000AtKV9QAN.png

and need to input like as below

0690X00000AtKVJQA3.png

My case is like as below.

0690X00000AtKVTQA3.jpg

my case, I cannot find inet4 addr and have inet6 addr.

So cannot use inet6 addr to /Startup/inet addr.

I have connected usb c cable with my laptop so also usb0 interface has inet addr so I put this addr at "/Startup/inet addr" and failed to work.

How can I get inet4 addr at eth0?

Is it due to usb connection or other issue?

Yli.8
Yli.8Author
Associate III
December 26, 2019

Thank you. My problem has been solved.The problem is that engineering mode is not set