Issue with RCC on flashing a blank project for STM32MP257F-DK
- 1 reply
- 892 views
Hello,
I have a stm32mp257f-dk and I would like to create an STM32Cube project for my board.
To be able to use the board, I have put in the eMMC the tsv file provided in the starter pack:
`en.FLASH-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.12.05/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.12.05/images/stm32mp2/flashlayout_st-image-weston/optee/FlashLayout_emmc_stm32mp257f-dk-optee.tsv`
My project aims to use the OpenAMP stack. I was able to flash the example which works very well but it does not have a .ioc file (which is necessary for my project).
So I used the STM32CubeMX Board Selector to generate an empty project.
First problem (screen 1), CubeMX tells me that DSIHOST, MDF1, and RCC are in conflict.
Since I don't need the Digital Filter and the screen, I disabled them.
I still have the RCC conflict. My code compiles but when flashing the project on the Cortex-M33, it crashes and here are the logs:
```
[ 34.029164] vddio3: disabling
[ 34.029233] vddio4: disabling
[ 34.029495] vdda18adc: disabling
[ 34.032767] v5v_vconn: disabling
[ 62.456994] ucsi-stm32g0-i2c 1-0035: i2c write 35, 08 error: -110
[ 62.481724] remoteproc remoteproc0: stopped remote processor m33
[ 65.806346] remoteproc remoteproc0: powering up m33
[ 65.892818] remoteproc remoteproc0: Booting fw image Project_PFE_CM33.elf, size 3320304
[ 65.895709] remoteproc remoteproc0: header-less resource table
[ 65.901623] remoteproc remoteproc0: no resource table found for this firmware
[ 65.908885] remoteproc remoteproc0: header-less resource table
[ E/TC:1 stm32_iac_itr:192 IAC exceptions [159:128]: 0x10000000
E/TC:1 stm32_iac_itr:197 IAC exception ID: 156
E/TC:1 Panic at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/drivers/firewall/stm32_iac.c:212 <stm32_iac_itr>
E/TC:1 TEE load address @ 0x82000000
E/TC:1 Call stack:
E/TC:1 0x82007ed8
E/TC:1 0x82041b44
E/TC:1 0x8202c2c0
E/TC:1 0x8203f678
E/TC:1 0x82013cf4
E/TC:1 0x820017dc
I/TC: Halting CPU 0
```
I checked the IAC exception 156 in the documentation and indeed it is related to RCC (screen 2). I see some logs inside the `/sys/kernel/debug/stm32_firewall/` directory.
I don’t really know what to do, I feel like I’m not heading in the right direction.
Would you have any idea knowing that I have not modified any code yet?