Skip to main content
EBelt.1
Associate II
September 18, 2021
Question

Issue building image for Azure IOT on STM32MP157C-DK2

I'm build an image for Azure IOT on STM32MP157C-DK2, following this tutorial: https://wiki.st.com/stm32mpu/wiki/How_to_integrate_Azure_IoT_Edge_on_OpenSTLinux

but I have follow error:

| error: attributes are not yet allowed on `if` expressions

|  --> /usr/src/debug/iotedge-daemon/1.1.6-r0/iotedge-1.1.6/vendor/sysinfo/src/utils.rs:27:5

|  |

| 27 |   #[allow(clippy::identity_conversion)]

|  |   ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

| 

| error: aborting due to previous error

| 

| error: could not compile `sysinfo`.

There is a possible solution?

Looking a similar issues, it seem a problem of version of Rust: https://github.com/Frederick888/git-credential-keepassxc/issues/12

There is a way to udate the Rust version used for build?

This topic has been closed for replies.

11 replies

darla14
Associate III
September 19, 2021

Hello,

have you installed all the dependencies needed for the Distribution package building?

Br,

EBelt.1
EBelt.1Author
Associate II
September 19, 2021

Yes, I did. once I make follow command:

DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh

it asked me all dependencies. I installed them and after when I re launch the command, it say was all ok and I started the build.

Can I ask witch versions of repository of those layers are tested in the tutorial?

PC $>git clone -b dunfell https://github.com/Azure/meta-iotedge.git

PC $>git clone git://github.com/meta-rust/meta-rust.git

PC $>git clone -b dunfell git://git.yoctoproject.org/meta-virtualization

I noticed that the are some update in repository meta-iotedge.git in date after the last update of article.

Jean-Marc B
ST Employee
September 20, 2021

Hello @EBelt.1​ 

to build Rust packages, I am using this repository:

https://github.com/rust-embedded/meta-rust-bin

It may help you. This layer supports Rust 1.54 and it is easy to upgrade to 1.55 (use the script build-new-version.sh).

Best regards,

--JM

EBelt.1
EBelt.1Author
Associate II
September 20, 2021

Thank you for your support. Just to understand (I'm pretty new to this builds), you say to replace those steps:

git clone git://github.com/meta-rust/meta-rust.git

bitbake-layers add-layer [your STM32MP1 Distribution path]/meta-rust/

with:

git clone https://github.com/rust-embedded/meta-rust-bin

bitbake-layers add-layer [your STM32MP1 Distribution path]/meta-rust-bin/

About that, I looking that has a specific branch for dunfell, instead meta-rust-bin has only for dizzy and zeus. What branch should I use? The master branch?

Jean-Marc B
ST Employee
September 20, 2021

@EBelt.1 

Yes, you can use the master branch. The compatibility layer as defined in conf/layer.conf includes dunfell.

Best regards,

--JM

EBelt.1
EBelt.1Author
Associate II
September 20, 2021

I tried to use meta-rust-bin, but the layer iot edge looks to depend on meta-rust:

ERROR: Layer 'meta-iotedge' depends on layer 'rust-layer', but this layer is not enabled in your configuration

Jean-Marc B
ST Employee
September 21, 2021

Hello @EBelt.1​ 

ok, I was not aware of this dependency. Too bad, the meta-rust-bin layer is quite quick ;)

To come back to your initial question, you can update the Rust compiler version by setting the variable RUST_VERSION = "1.55.0" (or other values) in your local.conf file.

About the versions used in the tutorial:

meta-iotedge : branch dunfell : commit 6840cf2afb51b4f2c535a05d5635736652f664f7
meta-virtualization : branch dunfell : commit 502b81ae3ae11bf4d889b7eff6239fb9e6c55994
meta-rust : branch master : commit e4d25b98083bcecb94df6ee189a165d63ede7f3d

The tutorial has been validated against the delivery ecosystem release v3.0.0 so be sure to used it.

Best regards,

--JM

EBelt.1
EBelt.1Author
Associate II
September 22, 2021

Thank you for the suggestion! I added RUST_VERSION = "1.55.0" to local.conf and aligned layers as suggested, but I had an error on building virtualitation (a repo was not found), but moving virtualitation to lastest everything work fine.

So, my final set was:

meta-iotedge : branch dunfell : commit 6840cf2afb51b4f2c535a05d5635736652f664f7

meta-rust : branch master : commit e4d25b98083bcecb94df6ee189a165d63ede7f3d

meta-virtualization : branch dunfell : latest commit

RUST_VERSION = "1.55.0" in local.conf

and I successfully build the image and connected to IOTedge.

I noticed that the version of Iotedge is 1.1, that has know issues. Is it possible to update to version 1.2 of iotedge?

Jean-Marc B
ST Employee
September 23, 2021

Hello @EBelt.1​ 

I am happy you successfully built your image! That's a good point!

About your last question to migrate from 1.1 to 1.2 for the layer iotedge, I don't know. I think you should make an attempt on your side and select this version in your cloned repository and re-do the build.

Best regards,

--JM

EBelt.1
EBelt.1Author
Associate II
September 23, 2021

Thank you.

I successfully build with latest version of iotedge with follow commits:

meta-virtualization = dunfell 9e9868ef3d6e5da7f0ecd0680fcd69324593842 (latest)

meta-iotedge   = 6840cf2afb51b4f2c535a05d5635736652f664f7 (latest)

meta-rust      = 4b151fa804b1e78af445037e4136c133ada40a0 (rust == 1.47)

Just a one more question:

I changed ROOTFS_PARTITION_SIZE in /layers/meta-st/meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc in order to increase the size of system partition (i.e. 8 gb), but once created the flash that change has not effect (the root partition is always 1.9 gb):

Filesystem   Size Used Avail Use% Mounted on

devtmpfs    147M   0 147M  0% /dev

/dev/mmcblk0p6 1.9G 1.6G 222M 88% /

tmpfs      214M  64K 214M  1% /dev/shm

tmpfs      214M 8.8M 205M  5% /run

tmpfs      214M   0 214M  0% /sys/fs/cgroup

tmpfs      214M  52K 214M  1% /tmp

/dev/mmcblk0p4  58M  14M  40M 27% /boot

tmpfs      214M 192K 214M  1% /var/volatile

/dev/mmcblk0p5  15M 6.8M 6.7M 51% /vendor

/dev/mmcblk0p7  13G 1.6G  11G 14% /usr/local

tmpfs      43M   0  43M  0% /run/user/0

how can I change the size of root partition?

Jean-Marc B
ST Employee
September 24, 2021

Hello @EBelt.1​ 

Once again a good piece of news!

About your questions related to the increase of the ROOTFS_PARTITION_SIZE, do you also update IMAGE_ROOTFS_MAXSIZE in the same file so its value is bigger or equal to ROOTFS_PARTITION_SIZE?

Hope it helps.

Best regards,

--JM