Skip to main content
Pratik Manvar
Associate II
September 30, 2021
Question

Issue booting with eMMC on STM32MP157F-Eval board

Hello STM-Team,

I am working with STM32MP157F-Eval board. The SD card and NAND booting are working fine. But, getting issues while booting with eMMC.

I have tried a workaround which seems to be working and I want to make sure if it is the right way of doing.

Please see below error. 

------------------------------------------------------------------------

Boot over mmc1!

Saving Environment to MMC... Writing to redundant MMC(1)... OK

switch to partitions #0, OK

mmc1(part 0) is current device

Scanning mmc 1:5...

Found U-Boot script /boot.scr.uimg

2943 bytes read in 29 ms (98.6 KiB/s)

## Executing script at c4100000

Executing SCRIPT on target=mmc1

Saving Environment to MMC... Writing to MMC(1)... OK

switch to partitions #0, OK

mmc1(part 0) is current device

Scanning mmc 1:5...

77087 bytes read in 30 ms (2.4 MiB/s)

SCRIPT FAILED... /mmc1_extlinux/extlinux.conf not found !

Saving Environment to MMC... Writing to redundant MMC(1)... OK

SCRIPT FAILED: continuing...

77087 bytes read in 31 ms (2.4 MiB/s)

STM32MP>

STM32MP> ls mmc 1:5 /

<DIR>    1024 .

<DIR>    1024 ..

<DIR>   12288 lost+found

      2943 boot.scr.uimg

<DIR>    1024 mmc0_extlinux

<DIR>    1024 nand0_extlinux

      18244 splash.bmp

      77374 stm32mp157f-ev1-a7-examples.dtb

      77607 stm32mp157f-ev1-m4-examples.dtb

      77087 stm32mp157f-ev1.dtb

     7309840 uImage

     3632420 uInitrd

STM32MP> ls mmc 1:5 /mmc0_extlinux/

<DIR>    1024 .

<DIR>    1024 ..

       256 extlinux.conf

       706 stm32mp157f-ev1_extlinux.conf

STM32MP>

------------------------------------------------------------------------

I am suspecting 2 probable issues while booting with eMMC on STM32MP157F-Eval board.

1. Below u-boot environments are wrong.

---------------------------------------------

boot_syslinux_conf=extlinux/extlinux.conf

boot_prefixes=/ /boot/

boot_targets=mmc1 ubifs0 mmc0 mmc2 pxe

---------------------------------------------

So, I have updated and saved the environments as below.

---------------------------------------------

STM32MP> setenv boot_syslinux_conf 'extlinux\/stm32mp157f-ev1_extlinux.conf'

STM32MP> setenv boot_prefixes '/mmc0_' // As 'stm32mp157f-ev1_extlinux.conf' stored in 'mmc0_extlinux' directory.

STM32MP> setenv boot_targets mmc1

STM32MP> saveenv

---------------------------------------------

2. It always append bootargs (root=PARTUUID) of mmc0 (sdcard) instead of mmc1.

---------------------------------------------

append: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200

---------------------------------------------

So, I have commented the 'set_env' function in bootloader source and changed bootargs at runtime as below as per  "https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#GPT_partuuid_of_rootfs_partition". 

---------------------------------------------

STM32MP> setenv bootargs 'root=PARTUUID=491f6117-415d-4f53-88c9-6e0de54deac6 rootwait rw console=ttySTM0,115200'

---------------------------------------------

After doing above two stuff, board is booting fine with eMMC.

I am wondering why the build is configured to refer to mmc0 (SDcard) instead of mmc1 (eMMC)?

Thank You.

Regards,

Pratik Manvar

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
October 1, 2021

Hi @Pratik Manvar​ ,

Can you please detail how did you build this faulty image ?

Distribution or Development package ?

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Pratik Manvar
Associate II
October 1, 2021

Hi @Community member,

Thanks for the reply.

I am using the distribution package (openstlinux-5.4-dunfell-mp1-20-06-24) and building for evaluation board "MACHINE=stm32mp1-eval".

I have some updates. With clean build (removed old build directory), I don't see above issues.

The default boot device was BOOTDEVICE_LABELS += "sdcard" in "machine/stm32mp1-eval.conf" file. Which worked fine.

Then I had enable below config to test NAND flash boot-up. Which worked fine.

BOOTDEVICE_LABELS += "nand-4-256"

After that, I had enable below config to test eMMC flash boot-up. In which I came across above issues.

BOOTDEVICE_LABELS += "emmc"

To generate above build images (NAND & eMMC), I had run below commands without deleting build directory (build-openstlinuxweston-stm32mp1-eval).

$ DISTRO=openstlinux-weston MACHINE=stm32mp1-eval source layers/meta-st/scripts/envsetup.sh

$ bitbake st-image-weston -c cleansstate

$ bitbake st-image-weston

With this, NAND boot worked and eMMC boot didn't work.

But, after deleting build directory (build-openstlinuxweston-stm32mp1-eval) and with fresh build, I don't see such issues booting with eMMC. Everything works fine.

Thanks & Regards,

Pratik Manvar