Skip to main content
HMüll.4
Senior
Mar 25, 2025 10:44 AM UTC
Solved

isolcpus kernel parameter is ignored - make use of one STM32MP257 core only?

Hi,

I'm trying to run the whole ST-Linux-stuff on one core only to have the other one available for a time-consuming application. However, it seems the kernel-parameter isolcpus is not used, dmesg gives an output

[ 0.000000] Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw earlycon console=ttySTM0,115200 isolcpus=0
[ 0.000000] Unknown kernel command line parameters "isolcpus=0", will be passed to user space.
[ 2.309368] isolcpus=0

The message is correct, also with this parameter set, the processes are spread over all cores.

What could be the problem here? 

Thanks!

 

This topic has been closed for replies.
Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
Mar 28, 2025 9:11 AM UTC

Hello @HMüll.4 ,
I find it strange that you have this warning on your second line. I have it too using the same command line parameter as you have. However, using 1 as parameter, the warning is not here anymore and it seems to have the expected result.
Can you please make a try with isolcpus=1 instead of 0 ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
Mar 28, 2025 9:11 AM UTC

Hello @HMüll.4 ,
I find it strange that you have this warning on your second line. I have it too using the same command line parameter as you have. However, using 1 as parameter, the warning is not here anymore and it seems to have the expected result.
Can you please make a try with isolcpus=1 instead of 0 ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.