Skip to main content
NPete.3
Associate
December 8, 2022
Question

Is there any STM MCU/MPU which can be used for computer vision applications

Is there any STM MCU/MPU which can be used for computer vision applications such as face recognition, Object detection/tracking? If so, how much flash memory required to process video with 5MP camera at 30FPS?

Is there any STM MCU/MPU which can be used for AR/VR applications?

This topic has been closed for replies.

2 replies

TDK
December 9, 2022

The STM32MP series is more suited. But even more suited would be a full blown computer.

5MP * 30fps * 3bpp = 3.6 GBps. Not processing that on an MCU.

"If you feel a post has answered your question, please click ""Accept as Solution""."
PatrickF
ST Employee
January 6, 2023

Hi @NPete.3​ 

please have a look to https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_OpenSTLinux_Expansion_Package

and more specifically https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_-_face_recognition_using_TensorFlow_Lite_C%2B%2B_API

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent