Skip to main content
Associate III
August 14, 2024
Solved

Is the SD Card required for the STM32MP257F-EV1

Hello, 

 

I am working on bringing up the STM32MP257F-EV1 Development board and have a question. I was wondering if the SD card is actually required or if it and the EMMC are completely interchangeable and the whole board can work off completely off the EMMC. 

 

Thanks!

Carson

This topic has been closed for replies.
Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
August 15, 2024

Hello @Carson ,
The evaluation board is made to demonstrate different features, such as booting from different flash memory. So yes you can completely ignore the SD card if you want to boot from eMMC. 

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
August 15, 2024

Hello @Carson ,
The evaluation board is made to demonstrate different features, such as booting from different flash memory. So yes you can completely ignore the SD card if you want to boot from eMMC. 

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CarsonAuthor
Associate III
September 18, 2024

Thanks Erwan!