Skip to main content
Senior
Jun 24, 2026 10:13 PM UTC
Solved

Is Samsung K4FBE3D4HM-TFCL LPDDR4 compatible with Micron MT53E1G32D2FW-046 WT:C

I’m looking for a replacement of MT53E1G32D2FW-046 WT:C because it’s out of stock.

So, I have found Samsung K4FBE3D4HM-TFCL LPDD4. From what I can see, it’s compatible with MT53E1G32D2FW-046 WT:C:

  • Same voltage
  • Same package
  • Same pinout
  • Single rank
  • Follows JEDEC standard

Are there anything else I need to know before making an order of that LPDDR4 memory?

ZAKARIA_C1Best answer
ST Employee
Jun 29, 2026 2:05 PM UTC

Hello ​@Windows,

Based on the information compared, I believe the Samsung reference should work, but just in case, there are other part numbers on the wiki that have already been validated by ST here is the link Validated DRAM on STM32 MPU portfolio - stm32mpu

Best Regards,
Zakaria

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

5 replies

ZAKARIA_C1Best answer
ST Employee
Jun 29, 2026 2:05 PM UTC

Hello ​@Windows,

Based on the information compared, I believe the Samsung reference should work, but just in case, there are other part numbers on the wiki that have already been validated by ST here is the link Validated DRAM on STM32 MPU portfolio - stm32mpu

Best Regards,
Zakaria

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
WindowsAuthor
Senior
Jun 29, 2026 3:20 PM UTC

Thank you ​@ZAKARIA_C1 

I will give those a try!

asadullah4571
Associate III
Jul 10, 2026 10:35 AM UTC

Hi ​@Windows ​@ZAKARIA_C1 

Previously Also i used the same RAM , due to out of stock , USED ISSI { 2 GB RAM } Pin to pIn compatible little be DDR integration Change LIKE RAM INFORMATION {SIZE , FREQUENCY, Diable the Linuxkernel2 form the Memory Region and RIF File} and it Successfully boot. 

WindowsAuthor
Senior
Jul 23, 2026 9:00 PM UTC

Thank you ​@asadullah4571 

 

I will do that. Giving you a reply later when I receive that memory.

Associate II
Jul 11, 2026 3:03 AM UTC

You may run calibration for DDR and check the setting when using new deivce