Skip to main content
JJérô.1
Associate II
June 22, 2022
Question

Is it possible to connect an IMX477 on the STM32MPU157F-dk2

  • June 22, 2022
  • 3 replies
  • 2448 views

Hello,

When I plugged the IMX477 on a USB port and I have the following msg:

[ 7307.355686] usb 2-1.3: new high-speed USB device number 5 using ehci-platform

[ 7307.519593] uvcvideo: Found UVC 1.00 device Arducam IMX477 HQ Camera (0c45:636d)

[ 7307.534627] input: Arducam IMX477 HQ Camera: Arduc as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.3/2-1.5

[ 7307.550269] usb 2-1.3: 3:1: cannot get freq at ep 0x84

[ 7308.295030] usb 2-1.3: 3:1: cannot get freq at ep 0x84

[ 7308.349280] usb 2-1.3: 3:1: cannot get freq at ep 0x84

This topic has been closed for replies.

3 replies

Olivier GALLIEN
ST Technical Moderator
July 11, 2022

Hi @JACQUES Jérôme​ ,

I'm not expert but I understand that such device may require some specific driver/support which does not looks to be by default in OpenSTLinux.

Which version of ecosystem are you using ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JJérô.1
JJérô.1Author
Associate II
July 11, 2022
Hello,
another question, issu it possible to connect the amicam1 with the stm32MPU157f-dk2?
Thanks a lot,
Jérôme
JJérô.1
JJérô.1Author
Associate II
July 11, 2022

Hi Olivier,

Thanks for you interest !

I'm using the 2.1. I see there is the 4.0 version maybe ....

A question Olivier, do you work in Sophia Antipolis ?

If yes, is it possible to have a meeting ?

Best regards,

Jérôme