Skip to main content
Associate II
May 25, 2025 11:09 AM UTC
Question

Integartion of SONA IF513 WIFI-BLUETOOTH MODULE WITH STM32MP257F-EV

I am about to integrate Ezurio sna module If 513 with the STM32MP257F-EV  another to provide wireless capabilities to my board. does any one try this before for any assistance. I am using mini PCIE  TO M.2 adapter  to connect.  so if there is any to assist me with a complete guide , I will appreciate,

 

Thank you.

This topic has been closed for replies.

3 replies

Pavel A.
May 25, 2025 12:49 PM UTC

Have you already set up Linux on the board? If you plug the module into the miniPCIe and run lspci, will it show up?

 

Associate II
May 25, 2025 1:18 PM UTC

the only thing I see is   00:00.0 PCI bridge: Synopsys, Inc. Device 0550 (rev 01)

Pavel A.
May 25, 2025 7:18 PM UTC

And you see the same without the module connected (and powered up)?

Can you connect the module to some other host system and compare results?