Skip to main content
AKuma.46
Associate II
December 2, 2022
Question

Installing Distribution package for 1st time.

Hi,

I was downloading and installing Distribution package for the 1st time following this link: https://wiki.st.com/stm32mpu-ecosystem-v3/wiki/STM32MP1_Distribution_Package

As I want version openstlinux-5.10-dunfell-mp1-21-03-31

After source sync there are no files present. May I know why its discarding?

root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31# repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.10-dunfell-mp1-21-03-31

.repo/manifests/: discarding 3 commits

Your identity is: ***.*** [removed by moderator]

If you want to change this, please re-run 'repo init' with --config-name

Testing colorized output (for 'repo diff', 'repo status'):

 black  red   green  yellow  blue   magenta  cyan   white

 bold   dim   ul    reverse

Enable color display in this user account (y/N)?

repo has been initialized in /

If this is not the directory in which you want to initialize repo, please run:

  rm -r //.repo

and try again.

root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31# repo sync

Fetching project openembedded-core

Fetching projects: 12% (1/8)

Fetching project meta-openembedded

Fetching projects: 25% (2/8)

Fetching project bitbake

Fetching projects: 37% (3/8)

Fetching project meta-st-openstlinux

Fetching projects: 50% (4/8)

Fetching project meta-st-stm32mp

Fetching projects: 62% (5/8)

Fetching project meta-qt5/meta-qt5

Fetching projects: 75% (6/8)

Fetching project meta-st-scripts

Fetching projects: 87% (7/8)

Fetching project meta-st-stm32mp-addons

Fetching projects: 100% (8/8)

Fetching projects: 100% (8/8), done.

Syncing work tree: 100% (8/8), done.

layers/meta-openembedded/: discarding 137 commits

layers/meta-qt5/: discarding 6 commits

layers/meta-st/meta-st-openstlinux/: discarding 24 commits

layers/meta-st/meta-st-stm32mp/: discarding 36 commits

layers/meta-st/meta-st-stm32mp-addons/: discarding 4 commits

layers/meta-st/scripts/: discarding 2 commits

layers/openembedded-core/: discarding 587 commits

layers/openembedded-core/bitbake/: discarding 23 commits

root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31# ls

root@si-rd22:/distribution-package/openstlinux-5.10-dunfell-mp1-21-03-31#

Thankyou

This topic has been closed for replies.

1 reply

Gregory PLANCHON
ST Technical Moderator
December 20, 2022

Hello,

I recommend you to use the latest version of the distribution package.

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.