Skip to main content
kKim.1
Associate II
February 1, 2023
Solved

Install Ubuntu 18.04 (LTS) on STM32MP157D-EV1 board with starter package installed

I am using the STM32MP157D-EV1 board.

The starter package is currently installed in EMMC boot mode.

the version is "ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23 \n \l" .

I need to install Ubuntu 18.04 on this board, but I don't know how. 

Do I have to delete the installed package now and install Ubuntu 18.04?

Ah, I downloaded the ubuntu-18.04.6-desktop-amd64.iso file. 

I can use Windows 10 and Oracle virtualbox.

I want to use Windows 10 if possible, but if it's impossible, I can also use Oracle virtualbox.

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
February 2, 2023

Hi @kKim.1​ ,

"I need to install Ubuntu 18.04 on this board"

This is not possible!

It looks like you mixed you PC / Host machine setup requiring Ubuntu 20.04 LTS and the STM32MP157D-EV1 target board which can only support the provided OpenSTLinux distribution.

Can you clarify ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
February 2, 2023

Hi @kKim.1​ ,

"I need to install Ubuntu 18.04 on this board"

This is not possible!

It looks like you mixed you PC / Host machine setup requiring Ubuntu 20.04 LTS and the STM32MP157D-EV1 target board which can only support the provided OpenSTLinux distribution.

Can you clarify ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.