Skip to main content
KLock.2
Associate II
December 2, 2020
Question

In ST-Link32 Utility, Read Out Protection is Disabled, but I get the errors: The elf loader Program function fails. Memory-Loader error Error occured during program operation Programming error @ 0x08000B60!

I have the latest version of ST-Link Utility (ver. 4.6.0) on Windows 10 and the latest firmware (V2.J37.S7), both of which I downloaded yesterday. My co-worker has ST-Link Utility ver. 3.7.0 on Windows 7 and firmware V2.J24.S7 and he has no trouble writing to the device.

I'm having several other errors:

Blank check almost always fails. When I check the memory location where Blank Check fails, it looks right.

Sometimes (maybe 1 in 6 tries) the first file I try to load does load. But the second file NEVER loads. I get this error: Programming error @ 0x0800344C! (the memory address is always different.)

Read Out Protection is Disabled and no Flash sectors are protected.

I am using Program and Verify with Verify while programming selected.

Can you provide any assistance in programming this device? Is it possible to get the older version of ST-Link Utility and the older firmware?

This topic has been closed for replies.

1 reply

KLock.2
KLock.2Author
Associate II
December 2, 2020

Determined that the issues were caused by a bad cable.