Hi,
ST-Link is quite independant of the rest of the system, so your two issues are likely not linked.
1) For display issue,
please check potential misconnection of the display. Slightly press on the display on the opposite side of the screws.
See https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1/Let%27s_start/Unpack_the_STM32MP157x-EV1_board
Do you have the three green leds on the display ?
As an aternative to the ST-Link VCP console, playing with JP4 and JP5, you could use old fashioned DB9 UART connector (UART4 on motherboard) to see if the board correctly boot or provide error message. But if you see blue led, this mean uBoot is correctly started, so I'm confident on that.
2) For ST-Link, please check JP1. It must not be present to have ST-Link to work.
If you does not connect USB, but just power up the board (with CN1), the ST-Link LED LD6 should blink slowly.
If you does not power up the board (i.e. no CN1), but connect ST-Link USB, the ST-Link LED LD6 should bright fixed once enumerated.
You might also check behavior using the MB1263C board alone (i.e. removed from the motherboard).
Regards.
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent