Skip to main content
SLetter
Associate III
Mar 29, 2021 12:46 PM UTC
Solved

I have been following the instructions on the wiki to set up STM32CubeProgrammer on dk2. It appears I am missing port parameters. What is the correct command line?

I enter STM32_Programmer_CLI -c port=/dev/bus/usb/010/003 (lsusb reports this is correct) -w flashlayout_st-image-weston/trusted/Flashlayout_sdcard_stm32mp157c-dk2-trusted.tsv

udev drivers installed, Ubuntu 20.04

Warning: Wrong connect parameter:

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
Mar 29, 2021 3:58 PM UTC

Hi, just see that you mistyped the command, you miss the '-w'

should be : STM32_Programmer_CLI -c port=USB1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

I agree that the error message is not helping.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

9 replies

Ozone
Principal
Mar 29, 2021 1:32 PM UTC

Besides of documentation on the ST website ...

Did you try runtime help ?

I wouldn't expect a proper manpage from Windows-centered ST, but you can try with DOS/Windows standard "/?" as parameter.

SLetter
SLetterAuthor
Associate III
Mar 29, 2021 2:33 PM UTC

im On Ubuntu 20.4 command line, as far as I know there is no help?

PatrickF
ST Employee
Mar 29, 2021 2:47 PM UTC

Hi,

your 'port=' value is wrong, you should use first:

STM32_Programmer_CLI -l

to list available DFU interfaces.

Then use the 'Device Index' value in the command line, for instance:

STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/Flashlayout_sdcard_stm32mp157c-dk2-trusted.tsv

You could also use the CobeProgrammer GUI.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
SLetter
SLetterAuthor
Associate III
Mar 29, 2021 2:53 PM UTC

I tried that first like the instructions said. I got the very same error.

Warning: Wrong connect parameter: “flashlayout_st-image-weston/trusted/Flashlayout_sdcard_stm32mp157c-dk2-trusted.tsv�?

SLetter
SLetterAuthor
Associate III
Mar 29, 2021 2:57 PM UTC

letter@steve-T7500:~/work/Starter-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/images/stm32mp1$ !1955

STM32_Programmer_CLI -l usb

     -------------------------------------------------------------------

                       STM32CubeProgrammer v2.7.0                 

     -------------------------------------------------------------------

===== DFU Interface  =====

Total number of available STM32 device in DFU mode: 1

 Device Index          : USB1

 USB Bus Number        : 009

 USB Address Number    : 004

 Product ID            : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

 Serial number         : 0045002A3338510B39303435

 Firmware version      : 0x0110

 Device ID             : 0x0500

letter@steve-T7500:~/work/Starter-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/images/stm32mp1$ STM32_Programmer_CLI -c port=USB1 flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

     -------------------------------------------------------------------

                       STM32CubeProgrammer v2.7.0                 

     -------------------------------------------------------------------

Warning: Wrong connect parameter: "flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv"

USB speed  : High Speed (480MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

SN         : 0045002A3338510B39303435

FW version : 0x0110

Device ID  : 0x0500

Device name : STM32MP1

Device type : MPU

Device CPU : Cortex-A7

PatrickF
ST Employee
Mar 29, 2021 3:15 PM UTC

Hi, if "STM32_Programmer_CLI -l" :

  • does not work, please check again your PC prerequisites (Btw, did you use a native Linux PC or a Virtual Machine ?).
  • show "No STM32 device in DFU mode connected", please check board setup and connection.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
SLetter
SLetterAuthor
Associate III
Mar 29, 2021 3:29 PM UTC

Native Ubuntu 20.04. All prerequisites met, I can build the images, install them using the sdcard install script and have a working discovery board. I showed my results, I have a dfu mode device

PatrickF
PatrickFBest answer
ST Employee
Mar 29, 2021 3:58 PM UTC

Hi, just see that you mistyped the command, you miss the '-w'

should be : STM32_Programmer_CLI -c port=USB1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

I agree that the error message is not helping.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
SLetter
SLetterAuthor
Associate III
Mar 29, 2021 4:18 PM UTC

Thanks, yes, that is the issue.