Skip to main content
KevinA
Senior
January 14, 2020
Question

I can not find any 8 gigabit memory for the STM32MP157CAA3 What I have found is double the price of the processor! IS46TR16512BL ISSI and Micron ECF840AAACN-C1-Y3

I can not find any 8 gigabit memory for the STM32MP157CAA3 What I have found is double the price of the processor! IS46TR16512BL ISSI and Micron ECF840AAACN-C1-Y3

I was looking for 256X32 memory but gave up, found some 512X16 but this puts the the cost three times the napkin estimate, instead of $10 for memory it is $30, and that's if it is available !

This topic has been closed for replies.

7 replies

PatrickF
ST Employee
January 14, 2020

I agree that DDR are quite pricey this time, especially when going for small quantities thru distributors.

Note that IS46TR16512BL is Automotive grade, so higher price if not what you ask for.

8Gbit DDR3L x16 is not frequent, and we recommend to use 2x4Gbit devices in x32 (as on our STM32MP157C-EV1 board).

LPDDR has a price premium due to it's low power Vs DDR3L.

You also need to check if your application absolutely need 8Gbit, many embedded Linux products could run very well with a single 4Gbit x16

You could probably found MT41K256M16 at about 5$ (the one we have on our STM32MP157C-DK2 board).

Regards,

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
KevinA
KevinAAuthor
Senior
January 14, 2020

Our application is CNN with video and multiple cameras, yes I signed up for the AI Webinar.

KevinA
KevinAAuthor
Senior
January 14, 2020

I just found MT41K512M16HA-107 at Microns web site, Mouser stocks it and sells it in QTY 1, pricey but do-able... The question is why no DDR3 that is 32 bit wide?

PatrickF
ST Employee
January 14, 2020

DDR3L come initially from PC market and standardized by JEDEC. My understanding is that in order to reach high frequencies and high density on SODIMM, it is always easier to have multiple x8 or x16 devices to form a x32 or x64 bus, which keep the data lanes in point2point connection, instead of managing multiple rank (ChipSelects) which end up to very complex signal integrity for data lanes. Single die highest density is usually linked to technology node.

LPDDR2 or LPDDR3 come from mobile phone market, where size and power matters, so mostly x32 are available (usually is much finer ball pitch than DDR3L).

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
KevinA
KevinAAuthor
Senior
January 14, 2020

I was looking at the D2 schematic and it dawned on me to just add another 256X16 and hook the DQ16~DQ32 lines up. I can get the 256X16 for $3 each! Anyone see any reason this wouldn't work?

I'd have to tell the memory controller about the buss width is the only thing I see... but there something else, A15 is still not used, can I have two 512X16 which would require the A15 line and give me 2GB ?

Alex - APMemory
Associate II
December 8, 2023

fyi, if you look for 8Gb DDR3L x16 support at competitive price I'll suggest Zentel Japan A3T8GF43BBF-GML (https://www.zentel-japan.com/BeDownloadFiles/DSA3T8GF343BBFLF.06.pdf)

 

You can look at below link and sort by price, just as general reference & comparison purpose

https://eu.mouser.com/c/semiconductors/memory-ics/dram/?memory%20size=8%20Gbit&organization=512%20M%20x%2016&type=SDRAM%20-%20DDR3L&sort=pricing

Using 2 pces of 4Gb DDR3 remains obviously another solution

Alex