Skip to main content
SScar.2
Senior
May 24, 2024
Solved

How to write STM32MP153 registers (RCC_RDLSICR)?

Hi, 

I'm trying to change the value of the register RCC_RDLSICR (RCC reset duration and LSI control register, address offset 0x144). I need to change the Minimum Reset Duration value.

In all power management/low power handling manuals for STM32MP15x lines the documentation says that you can change the registers value, but I can't find HOW I can achieve that. 

I can write them in dts? inside u-boot? please I need clarifications about that. 

NOTE: I'm using a custom STM32MP153 board with OpenSTLinux distribution on it. 

 

Thanks a lot

This topic has been closed for replies.
SScar.2
SScar.2Best answer
Senior
June 3, 2024

Got IT!! 

---
 plat/st/stm32mp1/bl2_plat_setup.c | 10 +++++++---
 plat/st/stm32mp1/stm32mp1_ssp.c | 10 +++++++---
 2 files changed, 14 insertions(+), 6 deletions(-)

diff --git a/plat/st/stm32mp1/bl2_plat_setup.c b/plat/st/stm32mp1/bl2_plat_setup.c
index 6232d7b..795cefe 100644
--- a/plat/st/stm32mp1/bl2_plat_setup.c
+++ b/plat/st/stm32mp1/bl2_plat_setup.c
@@ -286,10 +286,14 @@ void bl2_el3_plat_arch_setup(void)
 	}
 
 	/* Set minimum reset pulse duration to 31ms for discrete power supplied boards */
-	if (dt_pmic_status() <= 0) {
-		mmio_clrsetbits_32(rcc_base + RCC_RDLSICR, RCC_RDLSICR_MRD_MASK,
+	// if (dt_pmic_status() <= 0) {
+	// 	mmio_clrsetbits_32(rcc_base + RCC_RDLSICR, RCC_RDLSICR_MRD_MASK,
+	// 			 31U << RCC_RDLSICR_MRD_SHIFT);
+	// }
+
+	//SS set minimum reset pulse duration MDR register to 31 ms for ALL configurations 
+	mmio_clrsetbits_32(rcc_base + RCC_RDLSICR, RCC_RDLSICR_MRD_MASK,
 				 31U << RCC_RDLSICR_MRD_SHIFT);
-	}
 
 	generic_delay_timer_init();
 
diff --git a/plat/st/stm32mp1/stm32mp1_ssp.c b/plat/st/stm32mp1/stm32mp1_ssp.c
index 14ce023..9900672 100644
--- a/plat/st/stm32mp1/stm32mp1_ssp.c
+++ b/plat/st/stm32mp1/stm32mp1_ssp.c
@@ -927,10 +927,14 @@ void bl2_el3_plat_arch_setup(void)
 	}
 
 	/* Set minimum reset pulse duration to 31ms for discrete power supplied boards */
-	if (dt_pmic_status() <= 0) {
-		mmio_clrsetbits_32(rcc_base + RCC_RDLSICR, RCC_RDLSICR_MRD_MASK,
+	// if (dt_pmic_status() <= 0) {
+	// 	mmio_clrsetbits_32(rcc_base + RCC_RDLSICR, RCC_RDLSICR_MRD_MASK,
+	// 			 31U << RCC_RDLSICR_MRD_SHIFT);
+	// }
+
+	//SS set minimum reset pulse duration MDR register to 31 ms for ALL configurations 
+	mmio_clrsetbits_32(rcc_base + RCC_RDLSICR, RCC_RDLSICR_MRD_MASK,
 				 31U << RCC_RDLSICR_MRD_SHIFT);
-	}
 
 	generic_delay_timer_init();
 
-- 
2.25.1

 I patched both bl2_plat_setup.c and stm32mp1_ssp.c and it works (yes, I bypassed the check of the pmic status/mode), now when I reset the board I can see 31ms on the signal. 

7 replies

PatrickF
ST Employee
May 24, 2024

Hi @SScar.2 

I think you have to adapt TF-A code.

I found some lines related to non-STPMIC case which modify this register.

https://github.com/STMicroelectronics/arm-trusted-firmware/blob/v2.8-stm32mp/plat/st/stm32mp1/bl2_plat_setup.c#L291

Regards,

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
SScar.2
SScar.2Author
Senior
May 24, 2024

Hi Patrick, 

thanks for the quick response! 

Our solution adopts STPMIC. I don't know if this is useful information... 

I could patch the TF-A, but please specify which file I should modify. I'm pretty new to tf-a and I never patched it.

Thanks again