Skip to main content
Wjian.1
Associate III
March 16, 2020
Question

How to use specifically to Cortex-M4 on DK2

I need to develop M4 and how do I configure system resources,for example,we need to configure uart on M4,the modification as follows,but it doesn't work:

&m4_rproc {
 m4_system_resources {
 status = "okay";
 };
 };
 &m4_uart3{
 status = "okay";
 };

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
March 16, 2020

Hi @Wjian.1​ 

Did you already refer to wiki user guide ?

https://wiki.st.com/stm32mpu/wiki/How_to_configure_system_resources#ADC_example

https://wiki.st.com/stm32mpu/wiki/Serial_TTY_device_tree_configuration

https://wiki.st.com/stm32mpu/wiki/USART_internal_peripheral

Note that MP1 has an usart3 not uart3 device.

STM32CubeMX can also help you to assigned and configure properly usart3 to M4

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Wjian.1
Wjian.1Author
Associate III
March 17, 2020

Hi:

So thanks!Thanks to your help, it works very well now.By the way,the channel data location is not part of the InterProcessor communication controller and is stored in shared memory.So how much Shared memory is there when the data is transferred with IPCC.