Skip to main content
ykim.3
Associate
October 18, 2022
Question

How to use RTL8363NB in STM32MP157?

In AN5031 Rev4,

Figure 49. Gigabit Ethernet 2-port switch example with VDD = 3.3 V (RTL8363NB-VG)

There is the RTL8363NB used, but I can't find the driver anywhere.

Can you provide the driver file or tell me where it is?

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
October 27, 2022

Hi @ykim.3​ ,

Driver supposed to be provided by Realtek .. and most of the time up-streamed in Linux kernel.

I would be surprise it was not already supported by our latest OpenSTlinux based on kernel 5.15 ?

Did you try a "menuconfig" then search for realtek or RGMII drivers ?

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.