Skip to main content
Owen Murphy
Associate
June 1, 2023
Question

How to use github example code with STM32MP157D-DK1

The STM32MP1 example code on github targets the STM32MP157C on the STM32MP157C-DK2 and STM32MP157C-EV1 eval boards, however both of those boards are obsolete. I am using the STM23MP157D-DK1 eval board.

How do I port the example code so that it targets the correct chip and eval board?

Specifically, I am trying looking at the OpenAMP example code:

https://github.com/STMicroelectronics/STM32CubeMP1/tree/master/Projects/STM32MP157C-DK2/Applications/OpenAMP

https://github.com/STMicroelectronics/STM32CubeMP1/

Thank you,

Owen

This topic has been closed for replies.

2 replies

Erwan SZYMANSKI
ST Technical Moderator
June 2, 2023

Hello @OMurp.1​ ,

Basically, it should not be very different. Platforms are really closed to each other, you just do not have native display on DK1 if I remember well, and maybe some minor functionalities also.

If you already have a BSP ready, and a CubeFW package in phase with the kernel that runs on your A7 cortex, I do not see blocker for you to setup your example.

Did you face some trouble with it ?

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Owen Murphy
Associate
June 2, 2023

Hi Erwan,

I ended up making a new project targeting the DK1 setup, using CubeMX with OpenAMP enabled. I was able to copy all the relevant code over to my new project, and it seems to work just fine. Thanks for the response.

-Owen