Skip to main content
Associate III
Oct 15, 2024 3:23 PM UTC
Question

How to use flexible external memory controller bus with external FPGA as a memory device?

Dear Sir, 

We are using stm32mp135f processor on our custom board. We want to interface flexible external memory controller bus with an external FPGA device. How this can be achieved? Are there any reference or example that you can provide? Is it possible to connect FPGA as an external device?

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
Oct 18, 2024 9:19 AM UTC

Hi @stack_shailesh 

yes, you could connect an FPGA to the FMC.

Usually, the FPGA need to emulate an SRAM async interface to expose FPGA memory mapped registers/memories.

Then there is STM32MP1 memory map range directly accessible by your Linux driver or else.

Please have a look to this example with a external Ethernet PHY connected to FMC, which could be seens a similar than FPGA use case:  https://wiki.st.com/stm32mpu/wiki/FMC_device_tree_configuration#DT_configuration_of_the_external_bus_interface_controller_-28board_level-29

 

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent