Skip to main content
FrancoB
Associate II
January 11, 2021
Question

How to use DDR3 with Cortex-A7 (STM32MP157C-DK2 - C++ project)?

Good morning,

I'm working on a C++ project to collect data from a peripheral sensor using the STM32MP157C-DK2.

The estimated amount of data is at least 100 MB, so I have to use the DDR3 to store these data and then trasmit them over Ethernet using at the moment ONLY Cortex-A7 (no M4).

The project is write in C++ language and NOT using CubeMX, so I'm asking how can I activate and use the DDR3.

I've read some tutorials/documents from various sources:

# https://www.st.com/en/microcontrollers-microprocessors/stm32mp157.html#documentation

# https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_principle#rpmsg_sdb_driver

# https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example

and consequently I wrote the code (you will find it here attached with the dts in the card partition called "bootfs"), but I always receive the cout message "Mapping param failed.".

What I've to modify in the main code and, eventually, how/where can I add/modify the missing dts data to the MP1?

This topic has been closed for replies.

3 replies

Olivier GALLIEN
ST Technical Moderator
January 19, 2021

Hi @FrancoB​ ,

Sorry, I'm a bit puzzled with description of your problem.

I understand you would like to achieve Ethernet transfer of data from a peripheral sensor on A7 Linux side right ?

M4 and A7 to M4 communication not involved right ?

But you refer to

# https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_principle#rpmsg_sdb_driver

# https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example

Which demonstrate only buffer exchange between A7 and M4 ...

Can you please clarify ?

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
FrancoB
FrancoBAuthor
Associate II
January 19, 2021
Dear Olivier,
thank you for your useful tips.
I provide your informations at the people involved
Thank you very mach.