Associate II
December 10, 2021
Question
How to troubleshoot remoteproc on STM32MP157C.
- December 10, 2021
- 5 replies
- 3073 views
I am getting an error in the kernel log when remoteproc tries to "set hold boot" during startup in Linux. The error is:
remoteproc remoteproc0: failed to set hold boot
remoteproc remoteproc0: releasing m4
stm32-rproc: probe of mlahb:m4@10000000 failed with error -3
After this I do not have remoteproc0 in the /sys/class/remoteproc folder. I have attached device tree and log file.
Can someone please suggest a possible cause.