Skip to main content
LMarq.4
Associate
June 7, 2022
Solved

How to stream camera over network

I am a beginner with STM32MPUs and I've been trying to follow the example: How to stream camera over network (can't add links because I'm a new member but it's in ST Wiki)

I'm trying to stream the video from an USB Webcam connected to the STM32MP157F-DK2 over the network to another Ubuntu PC running on a virtual machine.

Unfortunately it doesn work. When I run:

v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=-1 --stream-to=- 2>/dev/null | gst-launch-1.0 fdsrc ! jpegparse ! rtpjpegpay ! udpsink host=192.168.0.9 port=5000

I see the webcam's LED on and I get the following output:

Frame rate set to 10.000 fps
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...

Then, when I run the command below on the host PC side, nothing happens.

gst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=JPEG ! rtpjpegdepay ! jpegparse ! decodebin ! videoconvert ! autovideosink

I have been able to test the webcam and I can see the video on the DK2's display using the following command

gst-launch-1.0 v4l2src device="/dev/video0" ! videoconvert ! autovideosink

Any ideas on what could be wrong with my test?

This topic has been closed for replies.
OlivierK
OlivierKBest answer
ST Technical Moderator
June 10, 2022

Hi LMarq.4 (Community Member)

Can you double check that you can ping the host 192.168.0.9 from the target?

I reproduced the test on an MP15-EV1 board with the ov5640 sensor, using the ethernet over usb cable to the host.

On the Host side:

enxbc141b6e675f: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500

    inet 192.168.7.229

On target side:

root@stm32mp1:~# ifconfig 

usb0   Link encap:Ethernet HWaddr EA:FA:3B:72:75:98             

     inet addr:192.168.7.1 Bcast:192.168.7.255 Mask:255.255.255.0     

 Target side:    

root@stm32mp1:~# v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,heigh

t=480,pixelformat=JPEG --stream-mmap --stream-count=-1 --stream-to=- 2>/dev/null

 | gst-launch-1.0 fdsrc ! jpegparse ! rtpjpegpay ! udpsink host=192.168.7.229 po

rt=5000                                     

Frame rate set to 30.000 fps                           

Setting pipeline to PAUSED ...                          

Pipeline is PREROLLING ...                            

Pipeline is PREROLLED ...                            

Setting pipeline to PLAYING ...                         

New clock: GstSystemClock  

Host side:

$ gst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=JPEG ! rtpjpegdepay ! jpegparse ! decodebin ! videoconvert ! autovideosink

Setting pipeline to PAUSED ...

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

Then a gst-launch-1.0 pop up window pops up on host, displaying the video capture.

Rgds,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

OlivierK
OlivierKBest answer
ST Technical Moderator
June 10, 2022

Hi LMarq.4 (Community Member)

Can you double check that you can ping the host 192.168.0.9 from the target?

I reproduced the test on an MP15-EV1 board with the ov5640 sensor, using the ethernet over usb cable to the host.

On the Host side:

enxbc141b6e675f: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500

    inet 192.168.7.229

On target side:

root@stm32mp1:~# ifconfig 

usb0   Link encap:Ethernet HWaddr EA:FA:3B:72:75:98             

     inet addr:192.168.7.1 Bcast:192.168.7.255 Mask:255.255.255.0     

 Target side:    

root@stm32mp1:~# v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,heigh

t=480,pixelformat=JPEG --stream-mmap --stream-count=-1 --stream-to=- 2>/dev/null

 | gst-launch-1.0 fdsrc ! jpegparse ! rtpjpegpay ! udpsink host=192.168.7.229 po

rt=5000                                     

Frame rate set to 30.000 fps                           

Setting pipeline to PAUSED ...                          

Pipeline is PREROLLING ...                            

Pipeline is PREROLLED ...                            

Setting pipeline to PLAYING ...                         

New clock: GstSystemClock  

Host side:

$ gst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=JPEG ! rtpjpegdepay ! jpegparse ! decodebin ! videoconvert ! autovideosink

Setting pipeline to PAUSED ...

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

Then a gst-launch-1.0 pop up window pops up on host, displaying the video capture.

Rgds,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.