Skip to main content
Hammy
Associate III
October 7, 2022
Question

How to store the u-boot-env on mmc so that fw_printenv can access it.

The default configuration for the trusted defconfig has CONFIG_ENV_IS_NOWHERE=y . How can I store the u-boot-env on mmc such that fw_printenv can read it. When I took out CONFIG_ENV_IS_NOWHERE I am unable to get the boot process to u-boot. The last thing I get is

NOTICE: SP_MIN: v2.4-r1.0(debug):devtool-patched-5-g73e4b89f4-dirty
NOTICE: SP_MIN: Built : 19:06:02, Sep 21 2022
INFO: ARM GICv2 driver initialized
INFO: Set calibration timer to 60 sec
INFO: stm32mp1 IWDG1 is secure
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world
INFO: CPU 0 IT Watchdog 2
INFO: CPU : 0
INFO: sp_usr : 0x0
INFO: lr_usr : 0x0
INFO: spsr_irq : 0x0
INFO: sp_irq : 0x0
INFO: lr_irq : 0x0
INFO: spsr_fiq : 0x0
INFO: sp_fiq : 0x0
INFO: lr_fiq : 0x0
INFO: spsr_svc : 0x0
INFO: sp_svc : 0xc00fcf08
INFO: lr_svc : 0xc0174d5d
INFO: spsr_abt : 0x0
INFO: sp_abt : 0x0
INFO: lr_abt : 0x0
INFO: spsr_und : 0x0
INFO: sp_und : 0x0
INFO: lr_und : 0x0
INFO: spsr_mon : 0xa00001f3
INFO: sp_mon : 0x2ffd8a80
INFO: lr_mon : 0xc0174d5c
INFO: scr : 0x225
INFO: pmcr : 0x41072000

and then a watchdog timer. My gpt image looks like this.

EOF
part fsbl1 --source rawcopy --fstype=ext4 --fsoptions "noauto" --part-name=fsbl1 --sourceparams="file=${DEPLOY_DIR_IMAGE}/arm-trusted-firmware/tf-a-stm32mp157c-osd32mp1-system-controller-sdcard.stm32" --ondisk mmcblk --part-type 0x8301 --fixed-size 256K --align 17
part fsbl2 --source rawcopy --fstype=ext4 --fsoptions "noauto" --part-name=fsbl2 --sourceparams="file=${DEPLOY_DIR_IMAGE}/arm-trusted-firmware/tf-a-stm32mp157c-osd32mp1-system-controller-sdcard.stm32" --ondisk mmcblk --part-type 0x8301 --fixed-size 256K
part fip --source rawcopy --fstype=ext4 --fsoptions "noauto" --part-name=fip --sourceparams="file=${DEPLOY_DIR_IMAGE}/fip/fip-stm32mp157c-osd32mp1-system-controller-trusted.bin" --ondisk mmcblk --part-type 0x8301 --fixed-size 4096K
 
part --source rawcopy --sourceparams="file=${WORKDIR}/uboot.env" --ondisk "$ondisk_dev" --align $boot_env_align_kb --no-table
part --source rootfs --rootfs-dir ${WORKDIR}/bootfs.${BB_CURRENTTASK} --ondisk "$ondisk_dev" --fstype=vfat --label boot --align $alignment_kb --fixed-size ${MENDER_BOOT_PART_SIZE_MB} --active $boot_part_params
part --source rootfs --ondisk "$ondisk_dev" --fstype=${ARTIFACTIMG_FSTYPE} --label primary --align $alignment_kb --fixed-size ${MENDER_CALC_ROOTFS_SIZE}k $exclude_path_options
part --source rootfs --ondisk "$ondisk_dev" --fstype=${ARTIFACTIMG_FSTYPE} --label secondary --align $alignment_kb --fixed-size ${MENDER_CALC_ROOTFS_SIZE}k $exclude_path_options
part --source rootfs --rootfs-dir ${IMAGE_ROOTFS}/data --ondisk "$ondisk_dev" --fstype=${ARTIFACTIMG_FSTYPE} --label data --align $alignment_kb --fixed-size ${MENDER_DATA_PART_SIZE_MB}
bootloader --ptable gpt
EOF

My u-boot defconfig looks like

CONFIG_ARM=y
CONFIG_ARCH_STM32MP=y
CONFIG_TFABOOT=y
CONFIG_SYS_MALLOC_F_LEN=0x3000
# CONFIG_ENV_OFFSET=0x280000
# CONFIG_ENV_OFFSET_REDUND=0x2c0000
CONFIG_ENV_OFFSET=0x280400
CONFIG_ENV_OFFSET_REDUND=0x282400
# CONFIG_ENV_SECT_SIZE=0x40000
# CONFIG_ENV_OFFSET=0x280000
# CONFIG_ENV_OFFSET_REDUND=0x2c0000
CONFIG_TARGET_AXCEND_SYSTEM_CONTROLLER=y
CONFIG_CMD_STM32PROG=y
CONFIG_DEFAULT_DEVICE_TREE="stm32mp157c-osd32mp1-system-controller"
CONFIG_DISTRO_DEFAULTS=y
CONFIG_FIT=y
CONFIG_BOOTDELAY=1
CONFIG_BOOTCOMMAND="run mender_setup; run bootcmd_stm32mp"
CONFIG_SYS_PROMPT="u-boot> "
# CONFIG_CMD_BOOTD is not set
CONFIG_CMD_ADTIMG=y
# CONFIG_CMD_ELF is not set
CONFIG_CMD_EEPROM=y
CONFIG_CMD_ERASEENV=y
CONFIG_CMD_MEMINFO=y
CONFIG_CMD_MEMTEST=y
CONFIG_SYS_MEMTEST_START=0xc0000000
CONFIG_SYS_MEMTEST_END=0xc4000000
CONFIG_CMD_ADC=y
CONFIG_CMD_CLK=y
CONFIG_CMD_DFU=y
CONFIG_CMD_FUSE=y
CONFIG_CMD_GPIO=y
CONFIG_CMD_I2C=y
CONFIG_CMD_MMC=y
CONFIG_CMD_REMOTEPROC=y
CONFIG_CMD_SPI=y
CONFIG_CMD_USB=y
CONFIG_CMD_USB_MASS_STORAGE=y
CONFIG_CMD_BMP=y
CONFIG_CMD_CACHE=y
CONFIG_CMD_TIME=y
CONFIG_CMD_TIMER=y
CONFIG_CMD_PMIC=y
CONFIG_CMD_REGULATOR=y
CONFIG_CMD_EXT4_WRITE=y
CONFIG_CMD_MTDPARTS=y
CONFIG_CMD_UBI=y
# CONFIG_ENV_IS_NOWHERE=y
CONFIG_CMD_SAVEENV=y
CONFIG_ENV_IS_IN_MMC=y
CONFIG_SYS_REDUNDAND_ENVIRONMENT=y
CONFIG_SYS_RELOC_GD_ENV_ADDR=y
CONFIG_SYS_MMC_ENV_DEV=0
CONFIG_SYS_MMC_ENV_PART=3
CONFIG_ENV_SIZE=0x2000
CONFIG_STM32_ADC=y
CONFIG_CLK_SCMI=y
CONFIG_SET_DFU_ALT_INFO=y
CONFIG_USB_FUNCTION_FASTBOOT=y
CONFIG_FASTBOOT_BUF_ADDR=0xC0000000
CONFIG_FASTBOOT_BUF_SIZE=0x02000000
CONFIG_FASTBOOT_USB_DEV=1
CONFIG_FASTBOOT_FLASH=y
CONFIG_FASTBOOT_FLASH_MMC_DEV=1
CONFIG_GPIO_HOG=y
CONFIG_DM_HWSPINLOCK=y
CONFIG_HWSPINLOCK_STM32=y
CONFIG_DM_I2C=y
CONFIG_SYS_I2C_STM32F7=y
CONFIG_LED=y
CONFIG_LED_GPIO=y
CONFIG_DM_MAILBOX=y
CONFIG_STM32_IPCC=y
CONFIG_STM32_FMC2_EBI=y
CONFIG_I2C_EEPROM=y
CONFIG_DM_MMC=y
CONFIG_SUPPORT_EMMC_BOOT=y
CONFIG_STM32_SDMMC2=y
CONFIG_MTD=y
CONFIG_DM_MTD=y
CONFIG_SYS_MTDPARTS_RUNTIME=y
CONFIG_MTD_RAW_NAND=y
CONFIG_NAND_STM32_FMC2=y
CONFIG_MTD_SPI_NAND=y
CONFIG_DM_SPI_FLASH=y
CONFIG_SPI_FLASH_MACRONIX=y
CONFIG_SPI_FLASH_SPANSION=y
CONFIG_SPI_FLASH_STMICRO=y
CONFIG_SPI_FLASH_WINBOND=y
# CONFIG_SPI_FLASH_USE_4K_SECTORS is not set
CONFIG_SPI_FLASH_MTD=y
CONFIG_PHY_REALTEK=y
CONFIG_DM_ETH=y
CONFIG_DWC_ETH_QOS=y
CONFIG_PHY=y
CONFIG_PHY_STM32_USBPHYC=y
CONFIG_PINCONF=y
CONFIG_PINCTRL_STMFX=y
CONFIG_DM_PMIC=y
CONFIG_PMIC_STPMIC1=y
CONFIG_DM_REGULATOR=y
CONFIG_DM_REGULATOR_FIXED=y
CONFIG_DM_REGULATOR_GPIO=y
CONFIG_DM_REGULATOR_STM32_VREFBUF=y
CONFIG_DM_REGULATOR_STPMIC1=y
CONFIG_REMOTEPROC_STM32_COPRO=y
CONFIG_RESET_SCMI=y
CONFIG_DM_RNG=y
CONFIG_RNG_STM32MP1=y
CONFIG_DM_RTC=y
CONFIG_RTC_STM32=y
CONFIG_SERIAL_RX_BUFFER=y
CONFIG_SPI=y
CONFIG_DM_SPI=y
CONFIG_STM32_QSPI=y
CONFIG_STM32_SPI=y
CONFIG_TEE=y
CONFIG_OPTEE=y
# CONFIG_OPTEE_TA_AVB is not set
CONFIG_USB=y
CONFIG_DM_USB=y
CONFIG_DM_USB_GADGET=y
CONFIG_USB_EHCI_HCD=y
CONFIG_USB_EHCI_GENERIC=y
CONFIG_USB_GADGET=y
CONFIG_USB_GADGET_MANUFACTURER="STMicroelectronics"
CONFIG_USB_GADGET_VENDOR_NUM=0x0483
CONFIG_USB_GADGET_PRODUCT_NUM=0x5720
CONFIG_USB_GADGET_DWC2_OTG=y
CONFIG_DM_VIDEO=y
CONFIG_BACKLIGHT_GPIO=y
CONFIG_VIDEO_LCD_ORISETECH_OTM8009A=y
CONFIG_VIDEO_LCD_RAYDIUM_RM68200=y
CONFIG_VIDEO_STM32=y
CONFIG_VIDEO_STM32_DSI=y
CONFIG_VIDEO_STM32_MAX_XRES=1280
CONFIG_VIDEO_STM32_MAX_YRES=800
CONFIG_WDT=y
CONFIG_WDT_STM32MP=y
CONFIG_ERRNO_STR=y
CONFIG_FDT_FIXUP_PARTITIONS=y
CONFIG_LMB_RESERVED_REGIONS=16
CONFIG_BOOTCOUNT_ENV=y
CONFIG_BOOTCOUNT_LIMIT=y

but I can't seem to get it to boot.

This topic has been closed for replies.

3 replies

SMich.1
Senior
October 13, 2022

Hi,

do you got this while trying to flash the image?

Hammy
HammyAuthor
Associate III
October 13, 2022

Yes

SMich.1
Senior
October 13, 2022

Your problem not with u-boot env .

You cannot flash with mender compiled fsbl and fip . I mean that the first two files:

#Opt Id Name Type IP Offset Binary

- 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp153a-mx-usb.stm32

- 0x03 fip-boot FIP none 0x0 fip/fip-stm32mp153a-mx-trusted.bin

you need to build one time without mender layer save this files a side and then to make image with mender.