Skip to main content
Associate III
October 1, 2020
Solved

How to specify the address to load Cortex-M4 firmware?

I want to know how to specify the address to load Cortex-M4 firmware when U-Boot or Linux Kernel load the firmware of Cortex-M4 in Retention RAM.

​

And, how to specify the address to load Cortex-M4 firmware if I load the firmware of Cortex-M4 in Retention RAM and MCUSRAM separately?

​

In addition, if I load the firmware of Cortex-M4 in Retention RAM and MCUSRAM separately, is the swithing of RetentionRAM and MCUSRAM done by MPU without the programmer being aware of it?

This topic has been closed for replies.
HMasu.1Best answer
Associate III
October 12, 2020

I close this thread because resolved this problem myself.

H. Masuda​

2 replies

HMasu.1Author
Associate III
October 6, 2020

Is this thread's support over...?

​

I would be very grateful if you could support me.

Best Regards.

H. Masuda

HMasu.1AuthorBest answer
Associate III
October 12, 2020

I close this thread because resolved this problem myself.

H. Masuda​