Skip to main content
Gencay
Associate III
August 9, 2022
Solved

How to install an example flutter app to STM32MP157F-DK2

I`ve built st-image-weston for stm32mp157f-disco board with flutter and clang layer. Then I built SDK with:

bitbake core-image-weston -c populate_sdk

Then I installed SDK with

.tmp/deploy/sdk/core-image-weston-openstlinux-weston-stm32mp15-disco-x86_64-toolchain-4.0.1-snapshot.sh

After that I setup environment with

source /opt/st/stm32mp15-disco/4.0.1-snapshot/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
 
 
export CC=${CLANGCC}
 
export CXX=${CLANGCXX}

My question is how can I install a simple flutter app to my discovery board. What are the steps that I need to follow.

This topic has been closed for replies.
Joel
JoelBest answer
Associate II
August 25, 2022

@Gencay​ This is not a simple answer.

First it depends on what image type you have (runtime=debug, runtime=release, runtime=profile).

My experience is that running a Flutter app via debug on the STM32MP157F-DK2 is very slow. So I would avoid that for now.

If you have a runtime=release image, then you have to create an AOT image.

The steps used by meta-flutter to generate an AOT (release - libapp.so) is located here:

https://github.com/meta-flutter/meta-flutter/blob/kirkstone/classes/flutter-app.bbclass#L170

If you install the flutter-engine-<runtime flavor>-sdk-dev package to image, you can scp the engine_sdk.zip from /usr/share/flutter/engine_sdk.zip. This has required gen_snapshot to generate an AOT image.

So once you have the libapp.so you create your bundle folder on target. This can be in /tmp or wherever you have write access to.

Create this folder structure on target. data/flutter_assets is from your host build/flutter_assets folder.

<bundle folder>

data

flutter_assets

lib

libapp.so

For DRM run:

`flutter-pi --release <bundle folder>`

For Wayland run:

`flutter-auto --w=1920 --h=720 --b=<bundle folder>

I may have missed something but that's the general flow. Feel free to start a discussion here so other meta-flutter users can benefit:

https://github.com/meta-flutter/meta-flutter/discussions

Cheers,

Joel

3 replies

Olivier GALLIEN
ST Technical Moderator
August 25, 2022

Hi @Gencay​ ,

@Community member​ (Kudos to him ! )  share his Flutter project for MP1 here in this community :

https://community.st.com/s/project/a8g3W000000fxV5QAI/google-flutter-for-stm32mp1

I'm quite sure this will help you

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Joel
JoelBest answer
Associate II
August 25, 2022

@Gencay​ This is not a simple answer.

First it depends on what image type you have (runtime=debug, runtime=release, runtime=profile).

My experience is that running a Flutter app via debug on the STM32MP157F-DK2 is very slow. So I would avoid that for now.

If you have a runtime=release image, then you have to create an AOT image.

The steps used by meta-flutter to generate an AOT (release - libapp.so) is located here:

https://github.com/meta-flutter/meta-flutter/blob/kirkstone/classes/flutter-app.bbclass#L170

If you install the flutter-engine-<runtime flavor>-sdk-dev package to image, you can scp the engine_sdk.zip from /usr/share/flutter/engine_sdk.zip. This has required gen_snapshot to generate an AOT image.

So once you have the libapp.so you create your bundle folder on target. This can be in /tmp or wherever you have write access to.

Create this folder structure on target. data/flutter_assets is from your host build/flutter_assets folder.

<bundle folder>

data

flutter_assets

lib

libapp.so

For DRM run:

`flutter-pi --release <bundle folder>`

For Wayland run:

`flutter-auto --w=1920 --h=720 --b=<bundle folder>

I may have missed something but that's the general flow. Feel free to start a discussion here so other meta-flutter users can benefit:

https://github.com/meta-flutter/meta-flutter/discussions

Cheers,

Joel

Gencay
GencayAuthor
Associate III
September 12, 2022

I have unzip this file

/usr/share/flutter/engine_sdk.zip

, then I have

engine_sdk/sdk/clang_x64/gen_snapshot 

directory at the target. After this how can I generate my AOT image?