Hi S.Kamath (Community Member)
On OSTL DV4.1, natively I have libc 2.35 using the starter package.
libc6 is already the newest version (2.35-r0).
If you use an old OSTL version, the starter image supports debian package update/install.
Just plug the ethernet cable or configure the wifi connected to the net.
root@stm32mp1:~# apt-get install libc
Regards,
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.