Skip to main content
Associate III
October 7, 2020
Solved

How to get STM32Cube_FW_MP1_V1.2.0RC2?

want to exchange large data buffers with the coprocessor.

I have done following wiki page.

​

https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_example#Source_code

​

I want to analyze Cortex-M4 source code, So I have get following source code.

​

https://github.com/STMicroelectronics/logicanalyser

​

I want to build the source code, but README says that "Drivers and Middleware are not included in the project; current assumption is that STM32Cube_FW_MP1_V1.2.0RC2 package is located at the same level as the project root folder."

​

How can I get STM32Cube_FW_MP1_V1.2.0RC2?

Or I have to investigate how to build the source code without STM32Cube_FW_MP1_V1.2.0RC2?

Best Regards.

H. Masuda

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
October 9, 2020

Hi @HMasu.1​ ,

Sorry let consider this as a typo error STM32Cube_FW_MP1_V1.2.0RC2 is the actual available STM32Cube_FW_MP1_V1.2.0 release.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
October 9, 2020

Hi @HMasu.1​ ,

Sorry let consider this as a typo error STM32Cube_FW_MP1_V1.2.0RC2 is the actual available STM32Cube_FW_MP1_V1.2.0 release.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
HMasu.1Author
Associate III
October 11, 2020

@Community member​ ,

Thank you for your reply.

I understood that it means STM32Cube_FW_MP1_V1.2.0.

H. Masuda