Skip to main content
JPabl.1
Associate III
Nov 13, 2024 2:50 PM UTC
Solved

How to find the custom recipe created in yocto inside st-image-qt

I created a st-image-qt image using the STM32MP Distribution package and X-LINUX-QT add-on for the STM32MP157F-DK2 board.

I could flash this image using the dd command in Linux and my target board is running correctly.

On the other side, I created a qt quick app using qt 6.7.3(which I could test ok using qt creator) and now I need to add this qt app in my st-image-qt image. I can bitbake this custom recipe doing "bitbake mygui"

I created the custom layer and a custom recipe and added this custom layer to my bblayers. Then, I built the image again with this custom recipe and it worked ok.

The problem is that I'm expecting to find this qt app inside my bin directory, but I can't see it.

 

SUMMARY = "This is the GUI for Hespect Software medical device"
DESCRIPTION = "Recipe created by bitbake-layers"
LICENSE = "CLOSED"
SECTION = "Mysection"

DEPENDS += " qtbase \
 qtdeclarative-native \
 qtdeclarative \
 qtquick3d \
 qtcharts"
 
RDEPENDS_${PN} += "qtwayland"

EXTRA_OECMAKE += "-DCMAKE_PREFIX_PATH=${STAGING_DIR_HOST}${prefix}"

SRC_URI += "file://main.cpp"
SRC_URI += "file://CMakeLists.txt"
SRC_URI += "file://CMakeLists.txt.user"
SRC_URI += "file://Backendsensors.h"
SRC_URI += "file://Backendsensors.cpp"
SRC_URI += "file://brushfactory.h"
SRC_URI += "file://brushfactory.cpp"
SRC_URI += "file://Main.qml"

# Add SVG images from the assets/images folder
SRC_URI += "file://assets/images/battery-full.svg"
SRC_URI += "file://assets/images/battery-mid.svg"
SRC_URI += "file://assets/images/rss-low.svg"
SRC_URI += "file://assets/images/signal-full.svg"
SRC_URI += "file://assets/images/signal-mid.svg"
SRC_URI += "file://assets/images/battery-low.svg"
SRC_URI += "file://assets/images/rss-full.svg"
SRC_URI += "file://assets/images/rss-mid.svg"
SRC_URI += "file://assets/images/signal-low.svg"

 
S = "${WORKDIR}/mygui"

do_install () {
 install -d ${D}${bindir}
 install -m 0775 mygui ${D}${bindir}/
}

FILES_${PN} += "${bindir}/mygui"

inherit cmake_qt5

 

In my local conf file I added: IMAGE_INSTALL_APPEND += "mygui"

This topic has been closed for replies.
JPabl.1
JPabl.1Best answer
Associate III
Nov 17, 2024 1:51 AM UTC

The problem was in the syntax. Space at the beginning, and no space at the end works correctly 

 

IMAGE_INSTALL:append = " mygui" 

 

3 replies

Eldam
Senior
Nov 14, 2024 12:00 PM UTC

yop yop,

u should have a look at:

https://www.blaess.fr/christophe/yocto-lab/sequence-III-1/index.html

its written in french, quite easy language!

look a part :

Intégration de scripts shells

 

and from ure side:

 

IMAGE_INSTALL_APPEND += "mygui"

IMAGE_INSTALL_APPEND += " mygui" (note the space)

 

hope it helps!

 

JPabl.1
JPabl.1AuthorBest answer
Associate III
Nov 17, 2024 1:51 AM UTC

The problem was in the syntax. Space at the beginning, and no space at the end works correctly 

 

IMAGE_INSTALL:append = " mygui" 

 

JPabl.1
JPabl.1Author
Associate III
Nov 16, 2024 1:04 PM UTC

I added IMAGE_INSTALL_APPEND += " gui" and compiled the image. When flashing the board I look for /usr/bin/gui but can't find anything. The closes thing I could find is usr/share/examples/gui but it has a "rasterwindow" file, so I think it didn't work

 

Note: I tried building fresh so I'm using gui instead of mygui