Skip to main content
johnnyc
Associate II
January 18, 2023
Question

How to enable/disable pwr_sw1 and pwr_sw1 via sysfs?

We need to enable/disable pwr_sw1 and pwr_sw1 preferably via sysfs:

vdd_usb_sw: pwr_sw1 {
 regulator-name = "vdd_usb_sw";
};
 
vdd_sd_sw: pwr_sw2 {
 regulator-name = "vdd_sd_sw";
 regulator-always-on;
 regulator-boot-on;
 regulator-active-discharge = <1>;
};

How can we achieve this?

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
January 25, 2023

Hi @johnnyc​ 

Please refer to Regulator overview - stm32mpu

It's clearly state :

"The regulator framework offers a sysfs interface that can be used for monitoring. It is not possible to control a regulator via the sysfs."

Best practice is to use "consumers" mechanism of the regulator.

As soon as regulator is not used it's turn-off. ( as soon as you remove regulator-always-on policy )

I guess this could be achieve by using some dedicated kernel drivers.

If you detail further to what pwr_sw1 and pwr_sw2 are connected in your design and what you want to do. I can come back with further guidelines.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.