Skip to main content
Associate II
Nov 25, 2025 11:21 AM UTC
Question

How to enable a custom LVDS display

Hi I was trying to connect a custom LVDS display to my STM32MP257F-dk board but it does not seem to work,

 

The display has a resolution of 1024x600 pixel and also it uses "vesa-24" scheme, so i assume that i don't need to change the device tree as it matches the specification of the default display which is supplied with the dev kit. If otherwise please advice.

 

Please not that i am not using the touch panel of the display so the i2c connection of the dev kit are not connected to the display board can that disable the LVDS port ?

 

Is there any way to debug the LVDS display, Please advise in this matter.

 

Regards,

Samip

1 reply

Associate II
Dec 6, 2025 7:26 AM UTC

Hey can anyone help on this ?? I was hoping to get a reply.