Skip to main content
Senior II
Mar 6, 2025 10:31 AM UTC
Question

how to create and open pdf in qt using stm32mp157d-dk1

I have created a button in qt when I click on the button it has to create a pdf and also display the pdf.

i am developing an application where i have to store the user data in pdf called report and later view it 

please give me the steps on how to perform this and any examples related to it 

This topic has been closed for replies.

4 replies

Erwan SZYMANSKI
ST Technical Moderator
Mar 10, 2025 1:43 PM UTC

Hello @Sharan ,
STMicroelectronics brings the necessary support to develop and use your Qt application to make it run on the target, but this question sounds more like a Qt specific topic.

I think the Qt official documentation or Qt forum could help you more than we can.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SharanAuthor
Senior II
Mar 24, 2025 6:58 AM UTC

how to open a pdf file from my terminal in stm32mp157d-dk1

root@stm32mp15-disco:~# xdg open mydoc.pdf

-sh: xdg: not found

root@stm32mp15-disco:~# okular mydoc.pdf

-sh: okular: not found

root@stm32mp15-disco:~# evince mydoc.pdf

-sh: evince: not found

root@stm32mp15-disco:~# mupdf mydoc.pdf

-sh: mupdf: not found

root@stm32mp15-disco:~#

A.M.
Associate III
Mar 31, 2025 12:41 PM UTC

Seems there is an example how to read/show pdf in Qt:

https://doc.qt.io/qt-6/qtpdf-pdfviewer-example.html

For creating PDFs, there are tons of libraries, some of them open-source.

SharanAuthor
Senior II
Apr 15, 2025 6:38 AM UTC

I am using QT 5.15.13 for my stm32mp157d-dk1  and the image does not have any pdf opener and i have upgraded my qt to 6.7.3 can i use this version for developing application because when i use ssh and connect to the stm32mp and when i type qmake it shows 

using qt version 5.15.13 in /usr/lib