Skip to main content
GLaure
Associate III
June 3, 2022
Solved

How to configure PTP PPS out?

Hi!

 

I am trying to enable PTP on STM32F157 DK2 evaluation board.

 

From my understanding, pps_available should return 1, (if configured correctly).

 

root@stm32mp1:~# cat /sys/class/ptp/ptp0/pps_available 
0

I added "linuxptp" to the image:

IMAGE_INSTALL_append += " \
 linuxptp \
 "

I tried to follow the instructions for kernel 4.14:

https://community.st.com/s/question/0D50X0000BMG2RoSQL/how-do-i-enable-linuxptp-pps-output

 

To enable PPS Out, I also patched stm32mp-mp15-pinctrl.dtsi

diff --git a/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi b/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi
index 236d77e..1e74905 100644
--- a/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi
+++ b/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi
@@ -160,6 +160,7 @@
 	ethernet0_rgmii_pins_a: rgmii-0 {
 		pins1 {
 			pinmux = <STM32_PINMUX('G', 5, AF11)>, /* ETH_RGMII_CLK125 */
+				 <STM32_PINMUX('G', 8, AF11)>, /* ETH_PPS_OUT */
 				 <STM32_PINMUX('G', 4, AF11)>, /* ETH_RGMII_GTX_CLK */
 				 <STM32_PINMUX('G', 13, AF11)>, /* ETH_RGMII_TXD0 */
 				 <STM32_PINMUX('G', 14, AF11)>, /* ETH_RGMII_TXD1 */
@@ -191,6 +192,7 @@
 	ethernet0_rgmii_sleep_pins_a: rgmii-sleep-0 {
 		pins1 {
 			pinmux = <STM32_PINMUX('G', 5, ANALOG)>, /* ETH_RGMII_CLK125 */
+				 <STM32_PINMUX('G', 8, ANALOG)>, /* ETH_PPS_OUT */
 				 <STM32_PINMUX('G', 4, ANALOG)>, /* ETH_RGMII_GTX_CLK */
 				 <STM32_PINMUX('G', 13, ANALOG)>, /* ETH_RGMII_TXD0 */
 				 <STM32_PINMUX('G', 14, ANALOG)>, /* ETH_RGMII_TXD1 */
-- 
2.25.1

 

As far as I could see, the other changes are not longer needed for kernel 5.10.

 

Still cat /sys/class/ptp/ptp0/pps_available returns 0.

 

What did I miss?

 

Any help is greatly appreciated!

 

Have a nice weekend!

 

Gunther

This topic has been closed for replies.
OlivierK
OlivierKBest answer
ST Technical Moderator
July 4, 2022

Hi GLaure (Community Member),

In fact to get the PG8 clock to work you also need to launch a PTP synchronization first

1- install linuxptp on the DK2 :

root@stm32mp1:~# apt-get install linuxptp

2- launch the PTP synchro

root@stm32mp1:~# ptp4l -l 6 -m -i eth0 -p /dev/ptp0

3- change the duty cycle of the PPS clock for a close to 50% ratio

root@stm32mp1:~# echo "0 0 0 1 1" > /sys/class/ptp/ptp0/period 

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

10 replies

OlivierK
ST Technical Moderator
June 6, 2022

Hi GLaur.3 (Customer) 

Can I ask which OpenSTLinux version you use?

and if you can please dump the clk_summary:

root@stm32mp1-disco:~# cat /sys/kernel/debug/clk/clk_summary > log.txt

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GLaure
GLaureAuthor
Associate III
June 7, 2022

Hi @OlivierK

The used OpenSTLinux version is: openstlinux-5.10-dunfell-mp1-21-11-17

I am building the image based on st-image-core without graphical applications.

The device tree contains changes to enable FDCAN 1 & 2, SPI4, QSPI and FMC.

I attached the clk_summary.

Thank you for your fast response!

Gunther

OlivierK
ST Technical Moderator
June 7, 2022

Hi GLaur.3 (Community Member)

I've loaded the same version as you. Normally the ptp clock is alive:

root@stm32mp1:~# grep ethptp_k /sys/kernel/debug/clk/clk_summary

     ethptp_k          1    1    0  99000000     0   0 50000

For some reason, it doesn't show out. I need to go a step further..

Rgds

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GLaure
GLaureAuthor
Associate III
June 8, 2022

@OlivierK​ 

Hi!

Do you have know if a previous OpenSTLinux version had PTP PPS out working?

Bye Gunther

OlivierK
ST Technical Moderator
June 10, 2022

Hi GLaur.3 (Community Member)

As you discovered, some hints were done on kernel 4.19 + patches:

https://community.st.com/s/question/0D50X0000BMG2RoSQL/how-do-i-enable-linuxptp-pps-output

As for a HAL point of view, the PPS PTP has been verified, but not yet on the linux part.

Patches were merged on latest ostl v3.1 version, the PPS output clock has been fixed, but there are still missing information. We are investigating internally, I will soon let you know.

Regards

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
OlivierK
ST Technical Moderator
June 17, 2022

Hi GLaur.3 (Community Member)

I tried to follow this page https://www.kernel.org/doc/html/latest/driver-api/pps.html

I've rebuild the kernel (ostl v3.1) to include the pps support in kernel menuconfig (PPS debugging messages, Kernel timer client, PPS line discipline, PPS client using GPIO)

installing the pps-tools on target (after enabling the network on DK board)

root@stm32mp1:~# apt-get install pps-tools

probing the pps-ktimer module

root@stm32mp1:~# modprobe pps-ktimer                       

[ 745.191786] pps pps0: new PPS source ktimer                  

[ 745.194557] pps pps0: ktimer PPS source registered 

Then pps0 is available...

root@stm32mp1:~# ls /sys/class/pps/pps0/                     

assert clear dev echo mode name path power subsystem uevent  

Then a timestamp and sequence number appears.

root@stm32mp1:~# cat /sys/class/pps/pps0/assert                 

1655492903.016517289#721 

Then I am able to launch a pps test

root@stm32mp1:~# ppstest /dev/pps0 

trying PPS source "/dev/pps0"

found PPS source "/dev/pps0"

ok, found 1 source(s), now start fetching data...

source 0 - assert 1655493082.936502257, sequence: 894 - clear 0.000000000, sequence: 0

source 0 - assert 1655493083.976522050, sequence: 895 - clear 0.000000000, sequence: 0

source 0 - assert 1655493085.016511920, sequence: 896 - clear 0.000000000, sequence: 0

source 0 - assert 1655493086.056506553, sequence: 897 - clear 0.000000000, sequence: 0

source 0 - assert 1655493087.096503036, sequence: 898 - clear 0.000000000, sequence: 0

source 0 - assert 1655493088.136501043, sequence: 899 - clear 0.000000000, sequence: 0

...

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GLaure
GLaureAuthor
Associate III
June 20, 2022

Good Morning @OlivierK​ 

Thank you for your support! I will follow your instruction and report back!

Regards,

Gunther

OlivierK
OlivierKBest answer
ST Technical Moderator
July 4, 2022

Hi GLaure (Community Member),

In fact to get the PG8 clock to work you also need to launch a PTP synchronization first

1- install linuxptp on the DK2 :

root@stm32mp1:~# apt-get install linuxptp

2- launch the PTP synchro

root@stm32mp1:~# ptp4l -l 6 -m -i eth0 -p /dev/ptp0

3- change the duty cycle of the PPS clock for a close to 50% ratio

root@stm32mp1:~# echo "0 0 0 1 1" > /sys/class/ptp/ptp0/period 

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
OlivierK
ST Technical Moderator
August 5, 2022

Hi GLaure (Community Member),

Any feedback? have you progressed on this topic?

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GLaure
GLaureAuthor
Associate III
August 10, 2022

Good Morning @OlivierK​ ,

PTP was on hold as I had to get DMA from an FPGA running. This is working now, so will look into PTP again. I will report back :)

Update:

I used this kernel config fragment:

CONFIG_PPS=y
CONFIG_PPS_DEBUG=y
#
# PPS clients support
#
CONFIG_PPS_CLIENT_KTIMER=m
CONFIG_PPS_CLIENT_LDISC=m
CONFIG_PPS_CLIENT_GPIO=m

The CONFIG_PPS_CLIENT_KTIMER has to be configured as a module. If it is buildin (with 'y') pps0 as device is not created.

Then start ptp4l as you described:

ptp4l -l 6 -m -i eth0 -p /dev/ptp0

and set the pps duty cycle

echo "0 0 0 1 1" > /sys/class/ptp/ptp0/period

A oszilloscpe now shows the PPS!

Perfect and thank you @OlivierK​ 

Update 2:

Just to be complete:

This is not necessary:

modprobe pps-ktimer
  1. You have to patch the PPS out pin in the device tree (PG8 in my case)
  2. CONFIG_PPS=y my be necessary
  3. You have to run pp4l
  4. You have to configure /sys/class/ptp/ptp0/period

Bye, Gunther