Skip to main content
Associate
May 8, 2025 8:51 AM UTC
Question

How do you control the Standby2 mode on the STM32MP2 series?

I am using the STM32MP257F-DK board. By default, this board automatically boots when power is applied. If the wakeup button is held for about 15 seconds, the system powers off. A short press and release of the wakeup button generates an interrupt signal that can be used by the kernel.

I would like to change this behavior with the following custom setup:

  • When power or battery is applied, the board should not boot automatically.

  • The system should only boot if the wakeup button is pressed and held for a defined time (around 3 seconds).

  • After the system has booted, pressing and holding the wakeup button again for the same defined time (around 3 seconds) should trigger a power-off.

  • A short press and release of the button should continue to generate an interrupt signal usable by the kernel.

Based on the following documentation:

It seems that these changes can be implemented by modifying the linux-stm32mp, optee-os-stm32mp, and tf-a-stm32mp sources.

Could you please guide me on exactly how to configure or modify these sources to implement this custom power and wakeup behavior?

This topic has been closed for replies.