Skip to main content
Dat Tran
Senior II
May 3, 2023
Solved

How do we access GPIO port Z registers through devmem?

We can use devmem to read/write all gpio port registers except for portZ.

We know this port relates to secure. is there any way to remove secure feature on this port so we can use devmem on this port?

Thanks

This topic has been closed for replies.
Dat Tran
Dat TranBest answer
Senior II
May 3, 2023

I got it working,

The was because I did not enable GPIOZ in RCC_MP_AHB5ENSETR.

3 replies

waclawek.jan
Super User
May 3, 2023

What chip are you talking about?

JW

Dat Tran
Dat TranAuthor
Senior II
May 3, 2023

Hi, STM32MP151AAC3

we are using SPL uboot see that uboot already have these code.

/* GPIOZ: deactivate the security */

writel(BIT(0), RCC_MP_AHB5ENSETR);

writel(0x0, GPIOZ_SECCFGR);

We also use " /sys/class/gpio/" and turn on /off PZ5 just fine. But use devmem to read 0x54004000 which is portZ base then system crashed.

Dat Tran
Dat TranAuthorBest answer
Senior II
May 3, 2023

I got it working,

The was because I did not enable GPIOZ in RCC_MP_AHB5ENSETR.