Skip to main content
Spamfast
Associate II
July 30, 2021
Question

How do I control STM32MP157 Cortex-M4-only reset signal using a Segger J-Link or J-Trace?

I've asked Segger but I was wondering if anyone knows how to get a Segger J-Link/Trace to put only the M4 core on an STM32MP157 into reset and bring it back out?

This topic has been closed for replies.

1 reply

OlivierK
ST Technical Moderator
August 26, 2021

Hi,

You should indeed ask Segger directly, It seems J-link SDK, https://www.segger.com/products/debug-probes/j-link/technology/j-link-sdk/

can send reset command from the cmd prompt.

It should works for debug the CortexM4, with the STM32MP157 board set in Engineering boot mode (to connect only to the Cortex M4 through JTAG).

Some related topics also:

https://forum.segger.com/index.php/Thread/7557-ABANDONED-Can-t-connect-to-M4-core-of-STM32MP1-STM32MP157/

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.