Skip to main content
GeorgeR
Associate II
June 29, 2022
Question

How do I configure an stm32mp157c GPIO pin to output?

I have configured the pins for uart7 to communicate with our zwave chip.

in kernel-source/arch/arm/boot/dts/stm32mp157c-dk2.dts

&uart7{
 pinctrl-names = "default", "sleep";
 pinctrl-0 = <&uart7_pins_a>;
 pinctrl-1 = <&uart7_sleep_pins_a>;
 status = "okay";
 
 zwave {
 uart7-gpios = <&gpioi 5 GPIO_ACTIVE_LOW>,
 <&gpioi 7 GPIO_ACTIVE_LOW>,
 <&gpioc 7 GPIO_ACTIVE_LOW>;
 };
 /* USER CODE BEGIN uart7 */
 /* USER CODE END uart7 */
};

kernel-source/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi :

 uart7_pins_a: uart7-0 {
 pins1 {
 pinmux = <STM32_PINMUX('A', 15, AF13)>; /* UART7_TX */
 bias-disable;
 drive-push-pull;
 slew-rate = <0>;
 };
 pins2 {
 pinmux = <STM32_PINMUX('E', 7, AF7)>; /* UART7_RX */
 bias-disable;
 };
 };
 
 uart7_sleep_pins_a: uart7-sleep-0 {
 pins {
 pinmux = <STM32_PINMUX('A', 15, ANALOG)>, /* UART7_TX */
 <STM32_PINMUX('E', 7, ANALOG)>; /* UART7_RX */
 };
 };

I want to control the chip with three output GPIO pins (C7, I5, and I7).

When I bitbake this and load it on the board, the configuration does not change. For C

# gpiodetect
gpiochip0 [GPIOA] (16 lines)
gpiochip1 [GPIOB] (16 lines)
gpiochip2 [GPIOC] (16 lines)
gpiochip3 [GPIOD] (16 lines)
gpiochip4 [GPIOE] (16 lines)
gpiochip5 [GPIOF] (16 lines)
gpiochip6 [GPIOG] (16 lines)
gpiochip7 [GPIOH] (16 lines)
gpiochip8 [GPIOI] (12 lines)
gpiochip9 [GPIOZ] (8 lines)

gpiochip2 - 16 lines:
 line 0: unnamed unused input active-high
 line 1: unnamed kernel input active-high [used]
 line 2: unnamed kernel input active-high [used]
 line 3: unnamed unused input active-high
 line 4: unnamed kernel input active-high [used]
 line 5: unnamed kernel input active-high [used]
 line 6: unnamed unused input active-high
 line 7: unnamed unused input active-high
 line 8: unnamed kernel input active-high [used]
 line 9: unnamed kernel input active-high [used]
 line 10: unnamed kernel input active-high [used]
 line 11: unnamed kernel input active-high [used]
 line 12: unnamed kernel input active-high [used]
 line 13: unnamed unused input active-high
 line 14: unnamed unused input active-high
 line 15: unnamed unused input active-high

and I

gpiochip8 - 12 lines:
 line 0: unnamed unused input active-high
 line 1: unnamed unused input active-high
 line 2: unnamed unused input active-high
 line 3: unnamed kernel input active-high [used]
 line 4: unnamed unused input active-high
 line 5: unnamed kernel input active-high [used]
 line 6: unnamed kernel input active-high [used]
 line 7: unnamed kernel input active-high [used]
 line 8: unnamed kernel input active-high [used]
 line 9: unnamed unused input active-high
 line 10: unnamed unused input active-high
 line 11: unnamed "interrupt" input active-high [used]

Where and how can I change the GPIO pins?

Can I change them in the kernel-source/arch/arm/boot/dts/stm32mp157c-dk2.dts and/or in kernel-source/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi ?

Thanks in advance,

George

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
July 4, 2022

Hi @GeorgeR​ 

I'm not expert, but you should probably need to declare a driver in your 'zwave' section (something like "compatible = ....").

Or use a dummy device (i.e. no driver)

https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_kernel_space

Otherwise, without specific driver nor any DT, you could control any 'free' GPIO:

https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace

This method could be used from any code (e.g. C or python), see also https://community.st.com/s/question/0D53W00001UZllVSAT

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
GeorgeR
GeorgeRAuthor
Associate II
July 5, 2022

Thank you @PatrickF​, I will check out the information.

Regards,

@GeorgeR​