Hi @Gencay ,
It depends on the image you want to compile. If you compile st-image-weston, Qt5 is not built.
If you want to compile st-example-image-qt without Qt5, you can:
- modify the bitbake file st-example-image-qt to remove dependencies with Qt (not really a graceful solution).
- create your own bitbake image file to build with what you want inside (and so flutter extra installation etc...)
- Write your local conf to remove Qt dependencies from CORE_IMAGE_EXTRA_INSTALL and add the ones of Flutter.
We know that a community Yocto Flutter layer is available for our target. Regarding their way to process, they used the local.conf configuration method in the context of their tests.
Hope that it can help you.
Kind regards,
Erwan.
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.