Skip to main content
vbuon.1
Associate III
July 22, 2021
Question

how can i modify the script start_up_demo_launcher.sh so that it has my application?

hi,

i would like to modify the start_up_demo_launcher.sh script as well as the weston.ini file so that my application is started instead of the STM demo application. i would then like to add these files to my own distribution package so that i can flash the eval board w/ it.

can someone tell me where i can find these files in an STM download package so that i can build my own image to flash?

thanks,

vince

This topic has been closed for replies.

3 replies

Olivier GALLIEN
ST Technical Moderator
July 23, 2021

Hi @vbuon.1​ ,

Thanks for your post and welcome in MP1 world !

As with many other questions answer is already in our wiki documentation ;)

see https://wiki.st.com/stm32mpu/wiki/GTK_demo_launcher

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
vbuon.1
vbuon.1Author
Associate III
July 23, 2021

hi olivier,

thank you for you response. however, my question was not about how to add to my application to the demo launcher but how to replace it w/ my own. i would like to remove all of the components that make up the demonstration application and put in my own application. is there an article that describes how i can setup my own autolaunch scripts that i can deploy to the A7? i would like to be able to create my own start_up_demo_launcher.sh and my own weston.ini file.

thanks,

vince

Olivier GALLIEN
ST Technical Moderator
July 26, 2021

Hi @vbuon.1​ ,

Sorry, reply to fast and was confused by your title.

Did you get and are you familiar with Yoco distribution package ?

Once Distribution installed please look :

layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb

-> adding the package-group st-demo to its configuration

layers/meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-st-demo.bbappend

-> asking for recipe demo-launcher to be execute

layers/meta-st/meta-st-openstlinux/recipes-samples/demo/demo-launcher.bb

-> recipe for demo-launcher

layers/meta-st/meta-st-openstlinux/recipes-graphics/wayland/weston-init/weston.ini

-> weston.ini customization to call demo-launcher script at start.

So the basic approach would be to create a customize image following the model of "st-image-weston" replacing demo-launcher by your own application.

Following links can give useful pointers :

https://wiki.st.com/stm32mpu/wiki/How_to_add_a_customer_application

https://wiki.st.com/stm32mpu/wiki/How_to_create_your_own_image

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.