Skip to main content
Tomáš Juřena
Senior
August 2, 2021
Solved

How can I get the MMC timing spec higher than sd high-speed?

Hello,

I am having difficulties with the MMC bus and the external SDIO wifi module. We are using the wifi module jody-w263 from U-blox with the OSD32MP1, and the communication with the module works, but it is quite slow. The wifi module is capable of SDR 104 and DDR50 communication speeds, but I add the support to the DTS, the communication is broken and the device returns the -110 while initializing.

How can I add support for higher speeds?

I attach the working dts, dmesg, ios and caps, and relevant schematic.

Any suggestion will be appreciated.

Best regards,

Tomáš.

This topic has been closed for replies.
Bernard PUEL
Bernard PUELBest answer
ST Technical Moderator
October 22, 2021

HEre is a workaround patch. I will explain later on ...

75 replies

Tomáš Juřena
Senior
October 12, 2021

Hello,

I realized that I sent you the log without the sdmmc_vswitch patch (does nothing and returns 0). The correct log is attached.

Bernard PUEL
ST Technical Moderator
October 12, 2021

sorry but you need to have also:

sd-uhs-ddr50;

To force uhs mode. IT seems you don't have.

Tomáš Juřena
Senior
October 12, 2021

I thought that it is missing.

Just to make it clear, this log is generated with the following configuration:

&sdmmc3{
	pinctrl-names = "default", "opendrain", "sleep";
	pinctrl-0 = <&sdmmc3_pins_mx>;
	pinctrl-1 = <&sdmmc3_opendrain_pins_mx>;
	pinctrl-2 = <&sdmmc3_sleep_pins_mx>;
	status = "okay";
 
	/* USER CODE BEGIN sdmmc3 */
	arm,primecell-periphid = <0x10153180>;
	non-removable;
	no-sd;
	no-mmc;
	st,neg-edge;
	bus-width = <4>;
	vmmc-supply = <&v3v3>;
	sd-uhs-ddr50;
	vqmmc-supply = <&v1v8_ldo1>;
	mmc-pwrseq = <&wifi_pwrseq>;
	/* USER CODE END sdmmc3 */
};

sdmmc_vswitch

static int sdmmc_vswitch(struct mmci_host *host, struct mmc_ios *ios)
{
	unsigned long flags;
	u32 status;
	int ret = 0;
#if 0
	if (ios->signal_voltage == MMC_SIGNAL_VOLTAGE_180) {
		spin_lock_irqsave(&host->lock, flags);
		mmci_write_pwrreg(host, host->pwr_reg | MCI_STM32_VSWITCH);
		spin_unlock_irqrestore(&host->lock, flags);
 
		/* wait voltage switch completion while 10ms */
		ret = readl_relaxed_poll_timeout(host->base + MMCISTATUS,
						 status,
						 (status & MCI_STM32_VSWEND),
						 10, 10000);
 
		writel_relaxed(MCI_STM32_VSWENDC | MCI_STM32_CKSTOPC,
			 host->base + MMCICLEAR);
 
		spin_lock_irqsave(&host->lock, flags);
		mmci_write_pwrreg(host, host->pwr_reg &
				 ~(MCI_STM32_VSWITCHEN | MCI_STM32_VSWITCH));
		spin_unlock_irqrestore(&host->lock, flags);
	}
#endif
	return ret;
}

Bernard PUEL
ST Technical Moderator
October 12, 2021

No related to functional issue but I saw in this log and also in previous ones:

[  3.219869] mmci-pl18x 48004000.sdmmc: clocking block at 120000000 Hz

IT seems the SDMMC is clocked at 120MHz whereas it is supposed to be at 200Mhz (from your information above).

Tomáš Juřena
Senior
October 12, 2021

I saw that too, but not really sure, how it happened. The clock tree in cubeMX shows the value 200Mhz for SDMMC3.

Bernard PUEL
ST Technical Moderator
October 13, 2021

Could you please share the same but without the patch on sdmmc_vswitch() ?

We saw the init sequence looks better and the switch voltage procedure needs to be done (event if we will keep the same voltage).

Tomáš Juřena
Senior
October 13, 2021

Of course. The log is attached.

Bernard PUEL
ST Technical Moderator
October 14, 2021

For the clock strange value, could you please output the result of this command (just to double check RCC settings are ok):

> cat /sys/kernel/debug/clk/clk_summary

Tomáš Juřena
Senior
October 19, 2021

I think that the rate for the mmc3 is correct.

Bernard PUEL
ST Technical Moderator
October 19, 2021

yes it is.

Bernard PUEL
ST Technical Moderator
October 14, 2021

For the last trace, we are a bit confused because looking at the 5.4.56 code version and the trace, we are seeing some mismatch (some inconsistency between the behavior and what is in the code).

What is the code you had backported from the kernel 5.10 in to your baseline (based on kernel 5.4.56) ?

Tomáš Juřena
Senior
October 19, 2021

I did not make any modifications except the DTS, defconfig, and disabling the code inside of the sdmmc_vswitch. I only hope that I did not send you logs, that contains some of my debug messages that could mislead you.

I am attaching the bbappend file for the linux-stm32mp_5.4 and manifest file to check that the versions match.

Bernard PUEL
ST Technical Moderator
October 19, 2021

Next step for us is to to send you a debug patch to better see what really happens (between the mmc framework and the regulator framework). So if you confirm you are on 5.4.56 except for the stm32 sdmmc drivers. We can proceed.

Tomáš Juřena
Senior
October 19, 2021

Yes, the only change is the sdmmc_vswitch, but I can revert it anytime.

Bernard PUEL
ST Technical Moderator
October 20, 2021

Hello Tomas,

your yocto setup looks good.

Could you please:

  • revert "sdmmc_vswitch" hack
  • apply previous dts config:

vmmc-supply = <&v3v3>;

sd-uhs-ddr50;

vqmmc-supply = <&v1v8_ldo1>;

mmc-pwrseq = <&wifi_pwrseq>;

/* USER CODE END sdmmc3 */

  • activate dyn trace:

root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 loglevel=8 dyndbg="file drivers/mmc/* +p"

  • apply the attached debug patch

And send us back the log of the boot.

Thanks in advanced.

Tomáš Juřena
Senior
October 20, 2021

Hi Bernard,

I have done what you asked for and here is the log. I hope it helps to identify the issue.

Bernard PUEL
ST Technical Moderator
October 20, 2021

Hello Tomas,

Could you please apply these 3 patches as a tentative correction ? You can keep the debug patch + dyn trace on a first step.

Bernard PUEL
ST Technical Moderator
October 20, 2021